cancel
Showing results for 
Search instead for 
Did you mean: 

STM32C0 Can not Connect STMStudio After Upload Code

Embedded_Class
Associate

Hi Community,
I’m having an issue with connecting the STMStudio application.
When I plug the programmer USB into the computer, the connection works without any problems. However, if I upload code via Keil uVision, I am unable to reconnect to the STMStudio app unless I unplug and replug the USB.

My Keil Setup like is Below.

Embedded_Class_0-1735306833883.png

And My Programmer Connection

Embedded_Class_1-1735306908577.png

 

Is there any point that ı can not catch?

Thanks for supporters.

 

 

0 REPLIES 0