2019-03-20 7:54 PM
have a default location X. If want to update the code, i download it to location Y and expect the STM32 to start at location Y after reboot. However, the routine keeps rebooting from X. what am i missing?
2019-03-24 4:55 PM
I have hex file that the filesize is 40kByte. I am not clear about what the last line is.
2019-03-24 8:03 PM
Why is this such an uphill ski?
:020000040800F2 << SEGMENT ADDRESS INFO
:1000000058330020D5000008C1410008993E00087F << BODY DATA
:1000100000000000000000000000000000000000E0
:100020000000000000000000000000000F47000872
:10003000000000000000000065430008295E000881
:10004000E7000008E7000008BF450008E7000008D7
...
:1089F0000000000000000000000000000000000077
:108A00000000000000000000000000000000000066
:108A10000000000000000000000000000000000056
:108A20000000000000000000000000000000000046 << END OF BODY DATA
:04000005080000C12E << YOU COULD LOSE THIS 05 RECORD
:00000001FF << THIS 01 RECORD LINE AT THE END OF THE FILE
2019-03-25 10:53 AM
Which tool should I use? I used winhex for merging 3 hex files - bootloader, app1, app2.
Winhex does not display data as you showed.
2019-03-25 12:37 PM
Which tool should I use? I used winhex for merging 3 hex files - bootloader, app1, app2.
Winhex does not display data as you showed.
2019-03-26 3:08 AM
This is my hex file which is opened in STM32CubeProgrammer.
Could you please let me know where the last line is?
Thank you.
2019-03-26 6:33 AM
They are in ASCII, use notepad or some text editor