cancel
Showing results for 
Search instead for 
Did you mean: 

How can I generate help documentation for my MCU

Adam Hamilton
Senior

I am using an STM32F031 and I can't see specific documentation for the F03x type. All I have is F070, F072 and F091 MCU types.

The Low Level API functions do not map correctly. For example, I am trying to set the PLL clock source and the function to do so is LL_RCC_PLL_ConfigDomain_SYS

All three help docs show 3 parameters for the function, whereas the actual function call for my MCU has two parameters.

Ok, it seems Doxygen is used but when I try, I can't get the output correct. For the pre-processor part, I enter the MCU part number STM32F031x6 but I don't get what I expect.

Any help with knowing what to put in the different fields, or a document somewhere that explains how ST does it would be much appreciated

Cheers

2 REPLIES 2
Adam Hamilton
Senior

Bump

https://community.st.com/s/question/0D50X0000AFs71HSQR/user-manual

@Khouloud GARSI​  @Nawres GHARBI​ 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..