2022-09-19 4:21 AM
I have written a program for write a data in SD card and after that read it. but in my program F_open function returns Fr_DISK_ERROR error and jumps outside the loop and terminates the execution whereas i have declared and defined all the necessary things and files. My card is connected with SPI and i have declared it.
Anyone tell me how can it works....
2022-09-19 4:44 AM
I have attached the complete main code of our programme in which i am not getting ny output.
Please check this code also !!
void check_SD_interface(void)
// Reads & writes config.txt file on SD card
{
U8 au8Key_pressed, au8StoredVolume;
UINT aupN_bytes_rwPtr[1];
short aNBytes_to_write;
tKeyinfo_t atpKeyPressedInfo[1];
FRESULT aFResult;
send_str_to_debugUART_n_wait_till_sent("\r\nChecking SDC interface");
// Read / create config.txt file from SDC
f_mount(&USERFatFs, "" ,0) ; // Returns FR_OK even if there is no SD card!
// Mounting the file system forcefully does not return FR_OK even when SD card is present!!
aFResult = f_open(&USERFile, "config.txt", FA_READ);
if(aFResult != FR_OK)
{
// may be it is the first power on for this SD card
// Try to open file for WRITE
aFResult = f_open(&USERFile, "config.txt", (FA_WRITE | FA_CREATE_NEW));
if(aFResult == FR_OK)
{
// config file opened for writing
// Write {"Vol":5}
// f_write (FIL* fp, const void* buff, UINT btw, UINT* bw); // Write data to the file
// 01 2345 678
strcpy((char *)gu8pSdd_rw_buffer,"{\"Vol\":");
strcat((char *)gu8pSdd_rw_buffer, num_string(INIT_VOLUME_SETTING, UNSIGNED, 1, NO_DECIMAL));
strcat((char *)gu8pSdd_rw_buffer, "}");
aNBytes_to_write = strlen((char *)gu8pSdd_rw_buffer);
// Write data to the file
aFResult = f_write (&USERFile, (const void *)gu8pSdd_rw_buffer, aNBytes_to_write, aupN_bytes_rwPtr);
if(aFResult == FR_OK)
{
gB_sd_card_present = TRUE;
}
f_close(&USERFile);
} // config.txt file opened for writing
} // f_open() returned error
else
{
// config.txt file opened for reading
f_read(&USERFile, gu8pSdd_rw_buffer, SDD_SECTOR_SIZE, aupN_bytes_rwPtr);
if (*aupN_bytes_rwPtr >= 8)
{
// At least one config parm is there
if (strncmp((char *)(gu8pSdd_rw_buffer + 2), "Vol", 3) == 0)
{
// It is "Vol" parm, read gu8Set_volume value
gu8Set_volume = gu8Stored_volume = gu8pSdd_rw_buffer[7] - 0x30;
// ASSUMED that it is within limits
} // It is "Vol" parm
gB_sd_card_present = TRUE;
} // 8 or more char in config.txt file
} // config.txt file opened for reading
f_close(&USERFile); // Checking of SD card & reading/creating config.txt file is over
au8StoredVolume = INIT_VOLUME_SETTING;
if (gB_sd_card_present)
{
send_str_to_debugUART_n_wait_till_sent("\r\nSuccessfully read/created config.txt file on SDC");
}
else
{
send_str_to_debugUART_n_wait_till_sent("\r\nUnable to read/created config.txt file on SDC");
return;
}
while (1)
{
send_str_to_debugUART_n_wait_till_sent("\r\nPress Incr volume / Decrement volume key" \
"to read storedVolume from config.txt file on SDC and write it back");
// Remove any pending keys in the key Q
while (BSP_check_for_key_press(atpKeyPressedInfo)) osDelay(100);
// Wait for Incr vol / decr vol key
while (!BSP_check_for_key_press(atpKeyPressedInfo))
{
// No key pressed
// Check if user pressed Enter on debug terminal
if ((osEventFlagsGet(debugUartEventHandle) & EVT_ENTER_PRESSED) == EVT_ENTER_PRESSED)
{
osEventFlagsClear ( debugUartEventHandle,
(EVT_ESC_PRESSED | EVT_ENTER_PRESSED | EVT_Y_ENTER_PRESSED | EVT_N_ENTER_PRESSED));
// Start receiving char from index 0
return; // Test over
}
osDelay(10);
}
// A key pressed
aFResult = f_open(&USERFile, "config.txt", FA_READ);
if( aFResult == FR_OK)
{
f_read(&USERFile, (void *)gu8pSdd_rw_buffer, SDD_SECTOR_SIZE, aupN_bytes_rwPtr); // Assumed it returns FR_OK
au8StoredVolume = gu8pSdd_rw_buffer[7] - 0x30;
f_close(&USERFile);
}
au8Key_pressed = atpKeyPressedInfo->fu8Kb_val;
switch (au8Key_pressed)
{
case KBVAL_KEY_INCR_VOLUME:
if (gu8Set_volume < MAX_VOLUME) gu8Set_volume++;
copy_str_to_debugUart_tx_buffer("\r\nVolume: ");
cat_str_to_debugUart_tx_buffer(BSP_u16_to_str((U16)gu8Set_volume, REMOVE_LEADING_ZEROES));
break;
case KBVAL_KEY_DECR_VOLUME:
if (gu8Set_volume > MIN_VOLUME) gu8Set_volume--;
copy_str_to_debugUart_tx_buffer("\r\nVolume: ");
cat_str_to_debugUart_tx_buffer(BSP_u16_to_str((U16)gu8Set_volume, REMOVE_LEADING_ZEROES));
break;
} // switch (au8Key_pressed)
send_debug_tx_line_n_wait_till_sent();
// Write the modified gu8Set_volume to SDC
aFResult = f_open(&USERFile, "config.txt", FA_WRITE);
if(aFResult != FR_OK)
{
// File write error!
f_close(&USERFile);
send_str_to_debugUART_n_wait_till_sent("\r\nFile write error!");
return;
}
else
{
// config file opened for writing
// Write {"Vol":au8StoredVolume}
// f_write (FIL* fp, const void* buff, UINT btw, UINT* bw); // Write data to the file
// 01 2345 678
strcpy((char *)gu8pSdd_rw_buffer,"{\"Vol\":");
strcat((char *)gu8pSdd_rw_buffer, num_string(au8StoredVolume, UNSIGNED, 1, NO_DECIMAL));
strcat((char *)gu8pSdd_rw_buffer, "}");
aNBytes_to_write = strlen((char *)gu8pSdd_rw_buffer);
// Write data to the file
aFResult = f_write (&USERFile, (const void *)gu8pSdd_rw_buffer, aNBytes_to_write, aupN_bytes_rwPtr);
f_close(&USERFile);
if (aFResult == FR_OK)
{
send_str_to_debugUART_n_wait_till_sent("\r\nFile written successfully");
}
else
{
send_str_to_debugUART_n_wait_till_sent("\r\nFile write error!");
return;
}
} // config.txt file opened for writing
} // while (1)
}
// ----- end of check_SD_interface() -----
I have found error in the [[[aFResult = f_open(&USERFile, "config.txt", (FA_WRITE | FA_CREATE_NEW));
if(aFResult == FR_OK)]]] function and after getting the error execution goes to the end of the else statement.
2022-09-19 6:14 AM
Instrument DISKIO layer, understand why it fails. The file system is dependent on it functioning correctly.
2022-09-19 9:53 PM
@Community member But How Can I Check it ??
2023-03-04 11:28 AM
@SGoel.2 have you found the answer? can you attach your stm32 project here. I'm having same problem