HID USB Data to the STM32F4 DISCOVERY
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-03-11 3:15 AM
Dear people on the ST Forum.
I am currently working on configuring the STM32F4 DISCO board as a HID device that must send an receive data from a host (PC). I've managed to configure it as a HID mouse and altered the descriptors and reports to send 64byte packets to the PC.I get the correct data from the device, but when I try to send data to the device (YAT terminal) I get an undefinable error and the terminal closes.Here's what I added to the USB FS project generated in CubeMx so far to try to accomplish this. :Added an EPOUT descriptorand changed the wTotallength accordingly in the Conf.Desc. and checked the Descriptors and report descriptors in USBlyzer..... /* 34 */ //////////////////////EPOUT Descriptor /////////////////////// 0x07, /*bLength: Endpoint Descriptor size*/ USB_DESC_TYPE_ENDPOINT, /*bDescriptorType:*/ HID_EPOUT_ADDR, /*bEndpointAddress: Endpoint Address (OUT)*/ // VADIM 0x03, /*bmAttributes: Interrupt endpoint*/ HID_EPOUT_SIZE, /*wMaxPacketSize: 64 Byte max */ 0x00, 0x0A, /*bInterval: Polling Interval (10 ms)*/} ; Changed the report Descriptors:<code>__ALIGN_BEGIN static uint8_t HID_MOUSE_ReportDesc[HID_MOUSE_REPORT_DESC_SIZE] __ALIGN_END ={ 0x06, 0xAB, 0xFF, // Report Descriptor Raw Hid 0x0A, 0x00, 0x02, 0xA1, 0x01, 0x75, 0x08, 0x15, 0x00, 0x26, 0xFF, 0x00, 0x95, 0x40, 0x09, 0x01, 0x81, 0x02, 0x95, 0x40, 0x09, 0x02, 0x91, 0x02, 0xC0}; </code>Added a Data out function in the HID callback structure<code>static uint8_t USBD_HID_DataOut (USBD_HandleTypeDef *pdev, uint8_t epnum);.....USBD_ClassTypeDef USBD_HID = { USBD_HID_Init, USBD_HID_DeInit, USBD_HID_Setup, NULL, /*EP0_TxSent*/ NULL, /*EP0_RxReady*/ USBD_HID_DataIn, /*DataIn*/ USBD_HID_DataOut, /*DataOut*/ // <<<<<< NULL, /*SOF */ NULL, NULL, USBD_HID_GetCfgDesc, USBD_HID_GetCfgDesc, USBD_HID_GetCfgDesc, USBD_HID_GetDeviceQualifierDesc,}; </code>Declared the USBD_HID_DataOut function
but to my knowledge this function is never entered...<code>static uint8_t USBD_HID_DataOut (USBD_HandleTypeDef *pdev, uint8_t epnum){ //printf(''Received \r\n'') ; USBD_LL_PrepareReceive(pdev, //VADIM HID_EPOUT_ADDR, /* (uint8_t*)*/HID_Rx_Buffer, HID_EPOUT_SIZE ) ; return USBD_OK;} </code>And in USBD_HID_INIT opened EPOUT<code>static uint8_t USBD_HID_Init (USBD_HandleTypeDef *pdev, uint8_t cfgidx){ uint8_t ret = 0; /* Open EP IN */ USBD_LL_OpenEP(pdev, HID_EPIN_ADDR, USBD_EP_TYPE_INTR, HID_EPIN_SIZE); /* Open EP OUT */ USBD_LL_OpenEP(pdev, <<<<<<<<<<<<<<<< HID_EPOUT_ADDR, USBD_EP_TYPE_INTR, HID_EPOUT_SIZE); USBD_LL_PrepareReceive(pdev, <<<<<<<<<<<< HID_EPOUT_ADDR, (uint8_t*)HID_Rx_Buffer, HID_EPOUT_SIZE ) ;....</code>Does somebody have more experience with HID on the STM32F4 ? For know I can't figure this out..I followed the approach in this thread for USB HID on the STM32F105/107https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FSTM32F105107%20HID%20USB%20device%20SET_REPORT%2C%20GET_REPORT&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F...Thanks in Advance,Vadim , Student at Thomas More - De Nayer #hid #hid #hid-usb-report-out #!stm32f4-!epout-!hid-!usb #usb #usb #usb #!stm32 #hid
- Labels:
-
USB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-03-12 9:28 AM
Almost fine, as long as the code described on your post.
> Added an EPOUT descriptor and changed the wTotallength accordingly in the Conf.Desc. Did you change these descriptor fields, too? Interface descriptor - bNumEndpoints field: 1 --> 2 HID descriptor - wDescriptorLength: --> 0x001C Tsuneo- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-03-13 11:55 AM
Hi Tsuneo,
Thanks for the replyThats's right , I changed :-HID_MOUSE_REPORT_DESC_SIZE to 0x1C-numEndpoints to 2-wTotallength to 41I checked the desciptors in USBlyzer and they all seem to work out.I read in UM1021 p.39''The USBD_HID_SendReport can be used by the application to send HID reports, the HID driver, in this release, handles only IN traffic.''This worries me a bit as I'm not very comfortable editing lower level functions to make the library handle OUT trafficIn UM1734 on p.18 it says that :''The library passes all the non-standard requests to the class-specific code with the callbackpdev->pClass->Setup(pdev,req) function.''And sould copy the setup request info to the struct usb_setup_req(usbd_def.h). but when I try to send anything from YAT terminal it doesn't enter this function.AlsoHAL_PCD_IRQhandler is called around 119 times during enumeration and twice every time I call a sendreport. But the IRQ handler is never called when I try to send information from YAT to to the device. Not even as an ''Invalid interrupt''.
monitoring the USB traffic with USBcap in Wireshark it seems to send the packet to the correct device and the correct endpoint..Did I miss out on something ? It must be possible to receive data from the host in the HID class..Kind Regards,Vadim , Student at Thomas More - De Nayer- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-03-15 5:05 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-03-15 9:40 AM
Hi Ramjagadeep,
What I did before was start from a HID mouse project and changing the descriptors and report to configure it as a custom HID that could only send data to the terminal. After that trying to add an endpoint and USBD_HID_DataOut callback function, which didn't work out .. As you suggested I tried this approach in a new Costum HID project and it worked ! I can now send and receive data to/from my USB device through YAT terminal.Strange as I modified the Mouse project the same way as Tsuneo and used the same descriptors as in the working project. But why didn't the OTG_FS_IRQHandler even get called as I sent something. It is the hardware that triggers this right ? Maybe the hw wasn't enabled to trigger an interrupt at an incoming report..I will look into this further when I made more progress with my project.Thanks for the tip! I was struggling with this for a while now.