cancel
Showing results for 
Search instead for 
Did you mean: 

Hi have purchased B-L475E-IOT02A board ,i have erased the program which has loaded by default in that board . can u send me bin file or source code of the factory loaded program in which it was trying to connect AWS MQTT broker

Sshan.1
Associate II
1 ACCEPTED SOLUTION

Accepted Solutions
Guillaume K
ST Employee
5 REPLIES 5
Peter BENSCH
ST Employee

There is no B-L475E-IOT02A available, maybe you are talking a B-L475E-IOT01A?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Sshan.1
Associate II

Hi ,

I am using the B-L475E-IOT01A2C board and i am getting this message ...after this what next i should do ???

#

# AI Validation 3.2

#

Compiled with GCC 7.3.1

STM32 Runtime configuration...

 Device    : DevID:0x00000415 (STM32L4x6xx) RevID:0x00001007

 Core Arch.  : M4 - FPU PRESENT and used

 HAL version : 0x010b0000

 system clock : 80 MHz

 FLASH conf. : ACR=0x00000604 - Prefetch=False $I/$D=(True,True) latency=4

AI platform (API 1.1.0 - RUNTIME 4.1.0)

Found network "network"

Creating the network "network"..

Initializing the network

Network configuration...

 Model name     : network

 Model signature  : 0c4409ac77edf66cabac2e5ec04b2e65

 Model datetime   : Wed Feb 5 15:26:48 2020

 Compile datetime  : Feb 5 2020 15:28:25

 Runtime revision  : (4.1.0)

 Tool revision   : (rev-5.0.0) (5.0.0)

Network info...

 nodes       : 6

 complexity    : 517361 MACC

 activation    : 17408 bytes

 params      : 16284 bytes

 inputs/outputs  : 1/1

  I[0] float32, 3840 bytes, shape=(30,32,1)

  O[0] float32, 12 bytes, shape=(1,1,3)

-------------------------------------------

| READY to receive a CMD from the HOST... |

-------------------------------------------

# Note: At this point, default ASCII-base terminal should be closed

# and a stm32com-base interface should be used

# (i.e. Python stm32com module). Protocol version = 2.1

Guillaume K
ST Employee

Regarding your first question about the original software programmed in B-L475E-IOT01:

https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32cube-expansion-packages/x-cube-aws.html

click on "Get software"

Guillaume K
ST Employee

regarding B-L475E-IOT01A1 vs B-L475E-IOT01A2 it seems there's a difference in the Sub-GHz module mounted on the boards: one is 868 MHz and the other is 915 MHz. The frequency depends on your country.

Sshan.1
Associate II

HI All ,

I got the development board code and it is working !!

Thanks For the Support