cancel
Showing results for 
Search instead for 
Did you mean: 

HardFault_Handler when call prvPortStartFirstTask() in STM32H753

EddiePark
Associate II

I’m using NUCLEO STM32H753ZI.
I use ST ID: STM32cudeIDE
I have HardFault_Handler when call vTaskStart_Scheduler() using FreeRTOS

Could you please let me know how to resolve this issue?

hardfault.jpg

Below is the sample code

int main(void)
{

(void) HAL_Init();

/* Configure the system clock */
SystemClock_Config();

/* Enable the CPU Cache */
CPU_CACHE_Enable();

BaseType_t xReturned;
TaskHandle_t xHandle = NULL;

/* Create tasks /
xReturned = xTaskCreate(
Task_Code,
“SB”,
configMINIMAL_STACK_SIZE,
(void) NULL,
tskIDLE_PRIORITY+2U,
&xHandle
);
if( xReturned == pdPASS )
{
vTaskStartScheduler();
}
else
{
}
while(1);
13 REPLIES 13

The most obvious way: modify slightly your FreeRTOS so that it triggers some other unused interrupt vector instead of SVC to call vPortSVCHandler and start the 1st task. This will remove conflict but I'm not sure that SBSFU will do what you need in combination with FreeRTOS.

 

Hi.

Could you please let me know how to resolve this issue? 

Hard Fault happens in below code

1.jpg

Ah so now the fault occurs in a different place? please use the CubeIDE Fault analyzer to get more info on the reason of the fault. 

 

Hopefully SBSFU experts can look at this thread and clarify how SBSFU can coexist with FreeRTOS.

PavelA_0-1752826749561.png

 

Hi.

What should I do when I change like below?

#define SFU_ISOLATE_SE_WITH_MPU -> #undef SFU_ISOLATE_SE_WITH_MPU

Hardfault happens when I change like above.

 

1.jpg