HAL TIM IC Capturecallback on multiple functions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-03 2:01 PM
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim)
{
// If the Interrupt is triggered by 1st Channel
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1)
{
RPM_captured = 1;
}
if (RPM_captured)
{
indx_RPM = 0;
count_RPM = 0;
RPM_measure_average = 0;
/* increment the index until some useful data shows up */
while (RPM_data[indx_RPM] == 0) indx_RPM++;
/* Again at very high frequencies, sometimes the values don't change
* So we will wait for the update among the values
*/
while ((MIN((RPM_data[indx_RPM+1]-RPM_data[indx_RPM]), (RPM_data[indx_RPM+2]-RPM_data[indx_RPM+1]))) == 0) indx_RPM++;
/* RPM_measure_average is the difference in the 2 consecutive rise Time */
/* Assign a start value to RPM_measure_average */
RPM_measure_average += MIN((RPM_data[indx_RPM+1]-RPM_data[indx_RPM]), (RPM_data[indx_RPM+2]-RPM_data[indx_RPM+1]));
indx_RPM++;
count_RPM++;
/* start adding the values to the RPM_measure_average */
while (indx_RPM < (SamplesBlockSize))
{
RPM_measure_average += MIN((RPM_data[indx_RPM+1]-RPM_data[indx_RPM]), RPM_measure_average/count_RPM);
count_RPM++;
indx_RPM++;
}
/* Find the average RPM_measure_average, the average time between 2 RISE */
RPM_measure_average = RPM_measure_average/count_RPM;
indx_RPM = 0;
//motor_RPM = 60/((float)RPM_measure_average * 0.00000001);
motor_RPM = 60/(RPM_measure_average * 0.00000001);
platter_RPM = motor_RPM / belt_ratio;
RPM_captured = 0;
RPM_measured = 1;
}
Solved! Go to Solution.
- Labels:
-
STM32G4 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-04 5:29 AM
Hello @Giordano
To handle multiple timer interrupts separately using the HAL library in STM32, you have two main options. The first option is to use a single callback function and differentiate the interrupts by checking the timer instance and the active channel within the HAL_TIM_IC_CaptureCallback function (as mentioned by @Tesla DeLorean). The second option is to register separate user-defined callback functions for each timer using the HAL_TIM_RegisterCallback function.
For the first option, you can check htim->Instance and htim->Channel to identify which timer and channel triggered the interrupt.
For the second option, define your custom callback functions and register them for each timer after initializing the timers. Both methods ensure that you can handle interrupts from multiple timers effectively. Here is an example of both approaches:
Single Callback Function with Instance Check:
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim) {
if (htim->Instance == TIM4) {
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1) {
// Handle TIM4 Channel 1 interrupt
}
} else if (htim->Instance == TIM5) {
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1) {
// Handle TIM5 Channel 1 interrupt
}
}
}
Registered Callbacks for Each Timer:
void User_TIM4_IC_CaptureCallback(TIM_HandleTypeDef *htim) {
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1) {
// Handle TIM4 Channel 1 interrupt
}
}
void User_TIM5_IC_CaptureCallback(TIM_HandleTypeDef *htim) {
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1) {
// Handle TIM5 Channel 1 interrupt
}
}
void Register_Callbacks(void) {
HAL_TIM_RegisterCallback(&htim4, HAL_TIM_IC_CAPTURE_CB_ID, User_TIM4_IC_CaptureCallback);
HAL_TIM_RegisterCallback(&htim5, HAL_TIM_IC_CAPTURE_CB_ID, User_TIM5_IC_CaptureCallback);
}
int main(void) {
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_TIM4_Init();
MX_TIM5_Init();
Register_Callbacks();
while (1) {
// Main loop
}
}
Saket_Om
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-03 7:17 PM
Differentiate which TIM instance is being handled, perhaps move the globals into the instance
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
‎2025-02-04 5:29 AM
Hello @Giordano
To handle multiple timer interrupts separately using the HAL library in STM32, you have two main options. The first option is to use a single callback function and differentiate the interrupts by checking the timer instance and the active channel within the HAL_TIM_IC_CaptureCallback function (as mentioned by @Tesla DeLorean). The second option is to register separate user-defined callback functions for each timer using the HAL_TIM_RegisterCallback function.
For the first option, you can check htim->Instance and htim->Channel to identify which timer and channel triggered the interrupt.
For the second option, define your custom callback functions and register them for each timer after initializing the timers. Both methods ensure that you can handle interrupts from multiple timers effectively. Here is an example of both approaches:
Single Callback Function with Instance Check:
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim) {
if (htim->Instance == TIM4) {
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1) {
// Handle TIM4 Channel 1 interrupt
}
} else if (htim->Instance == TIM5) {
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1) {
// Handle TIM5 Channel 1 interrupt
}
}
}
Registered Callbacks for Each Timer:
void User_TIM4_IC_CaptureCallback(TIM_HandleTypeDef *htim) {
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1) {
// Handle TIM4 Channel 1 interrupt
}
}
void User_TIM5_IC_CaptureCallback(TIM_HandleTypeDef *htim) {
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1) {
// Handle TIM5 Channel 1 interrupt
}
}
void Register_Callbacks(void) {
HAL_TIM_RegisterCallback(&htim4, HAL_TIM_IC_CAPTURE_CB_ID, User_TIM4_IC_CaptureCallback);
HAL_TIM_RegisterCallback(&htim5, HAL_TIM_IC_CAPTURE_CB_ID, User_TIM5_IC_CaptureCallback);
}
int main(void) {
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_TIM4_Init();
MX_TIM5_Init();
Register_Callbacks();
while (1) {
// Main loop
}
}
Saket_Om
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-04 1:38 PM
Yesss!
Thank You. I was thinking the same, but used wrong syntax. Also tried with others suggestion on this syntax ... if (htim==&htim4) ..., but did not work. This "Instance" is new to me, I look after now. It works, but I also want to understand why.
I appreciate your help you gave!!
JG