cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_RCC_GetPCLK2Freq() in HAL_InitTick delivers half the frequency

mkrug
Associate III

Dear all, 

I just came across something strange. 

I debugged into the function HAL_InitTick() to better understand how the OS tick (SysTick) is managed if FreeRTOS is used. I'm using TIM16 for the SysTick of the OS. At the beginning of HAL_InitTick() the function HAL_RCC_GetPCLK2Freq() is called. The return value is used to set the systick timer (in my case TIM16 on a STM32L432 device). 

My clock configuration for my device is set for PCLK2 = 80MHz. However, the function HAL_RCC_GetPCLK2Freq() returns 40.000.000. So half of the actual frequency. In the following the prescaler is set to 3 and the period to 999. So for my understanding the timer period until it will reset to 0 and raise an interrupt will be ((40.000.000/3)*1000) *(1/40.000.000). So this gives me a totally wrong value that certainly is not the case (I'm actually sure for other reasons that my device runs at 80MHz instead of 40MHz). Here is how it looks like just before entering HAL_TIM_Base_Init().

mkrug_0-1736963263542.png

Any idea bout my misunderstanding?

Best Regards
Markus

4 REPLIES 4
Chris21
Senior

Is your SystemCoreClock value correct?

Do you call SystemCoreClockUpdate() after changing clock dividers?

mkrug
Associate III

Hi Chris, 

thanks for you reply.

Well, I work 100% with the STM32CubeIDE generated software for this part of my application and not changing anything in the HAL manually. So I guess the SystemCoreClock value is correct. I will try to double check that later.

Best Regards

Markus

gbm
Lead III

If PCLK is obtained by dividing HCLK, then timer clock frequency is 2xPCLK - it's written in the RefMan.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
Saket_Om
ST Employee

Hello @mkrug 

Could please share with us your system clock config?

If your question is answered, please close this topic by clicking "Accept as Solution".

Thanks
Omar