2018-12-19 7:51 AM
Hello,
I'm new to the forum.
I have a Nucleo-L476RG board and I use Keil with Keil::STM32L4xx_DFP 2.1.0 to program it.
During the debug I notice that after the HAL_I2C_Master_Transmit_IT(I2C_HandleTypeDef *hi2c, ...) function call the hi2c->XferSize and hi2c->XferCount are correctly set.
But in the HAL_I2C_MasterTxCpltCallback(I2C_HandleTypeDef *hi2c) callback, if I try to access to hi2c->XferSize and hi2c->XferCount are both 0x0000. So I can't retrieve the real bytes sent?
If I do the same work with the UART dirver all is ok. Why this different behavior?
Thanks in advance,
Antonio
2018-12-23 11:27 PM
I have similar problem. In the STM32HAL, getting the transferred count is not documented. So, I am spending time to sniffing source code, but the behavior is so confused.
Please tell me the "right way".
2019-01-03 2:05 AM
Hi,
I didn't find a solution up to now. I think this is a bug, but I'm new to the STM family, so I don't know how to report it.
If you find some solution, please, report it here.
Thank you,
Antonio
2019-01-29 2:46 AM
None knows a solution?