2022-08-30 7:20 PM
I write a simple blinking project on STM32F4 Discovery board.
It calls HAL_Delay() function for blinking effect on one LED.
But the code hanging when reach HAL_Delay().
When I debug, the HAL_Delay() stuck at while() loop in there.
Here my code :
#include <stm32f4xx.h>
int main()
{
RCC_OscInitTypeDef x0;
RCC_ClkInitTypeDef x1;
RCC_PLLInitTypeDef x2;
GPIO_InitTypeDef x3;
x2.PLLSource = RCC_OSCILLATORTYPE_HSE;
x2.PLLM = 10;
x2.PLLN = 250;
x2.PLLP = RCC_PLLP_DIV2;
x2.PLLQ = 5;
x1.ClockType = RCC_CLOCKTYPE_SYSCLK;
x1.SYSCLKSource = RCC_SYSCLKSOURCE_HSE;
x1.AHBCLKDivider = RCC_SYSCLK_DIV1;
x1.APB1CLKDivider = RCC_HCLK_DIV4;
x1.APB2CLKDivider = RCC_HCLK_DIV4;
x0.OscillatorType = RCC_OSCILLATORTYPE_HSE;
x0.HSEState = RCC_HSE_ON;
x0.PLL = x2;
x3.Pin = GPIO_PIN_13;
x3.Mode = GPIO_MODE_OUTPUT_OD;
x3.Pull = GPIO_PULLUP;
x3.Speed = GPIO_SPEED_FREQ_LOW;
HAL_Init();
HAL_RCC_OscConfig(&x0);
HAL_RCC_ClockConfig(&x1, 5);
__HAL_RCC_GPIOD_CLK_ENABLE();
HAL_GPIO_Init(GPIOD, &x3);
while(1)
{
HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_13);
HAL_Delay(1000);
}
}
2022-08-30 9:07 PM
In Keil C, I trace reversely the HAL_Init() functions. I guess it does not initial Systick completely.
At the end, one function in "core_cm4.h" is displayed blurry.
it's here :
/* ################################## SysTick function ############################################ */
/**
\ingroup CMSIS_Core_FunctionInterface
\defgroup CMSIS_Core_SysTickFunctions SysTick Functions
\brief Functions that configure the System.
@{
*/
#if defined (__Vendor_SysTickConfig) && (__Vendor_SysTickConfig == 0U)
/**
\brief System Tick Configuration
\details Initializes the System Timer and its interrupt, and starts the System Tick Timer.
Counter is in free running mode to generate periodic interrupts.
\param [in] ticks Number of ticks between two interrupts.
\return 0 Function succeeded.
\return 1 Function failed.
\note When the variable <b>__Vendor_SysTickConfig</b> is set to 1, then the
function <b>SysTick_Config</b> is not included. In this case, the file <b><i>device</i>.h</b>
must contain a vendor-specific implementation of this function.
*/
__STATIC_INLINE uint32_t SysTick_Config(uint32_t ticks)
{
if ((ticks - 1UL) > SysTick_LOAD_RELOAD_Msk)
{
return (1UL); /* Reload value impossible */
}
SysTick->LOAD = (uint32_t)(ticks - 1UL); /* set reload register */
NVIC_SetPriority (SysTick_IRQn, (1UL << __NVIC_PRIO_BITS) - 1UL); /* set Priority for Systick Interrupt */
SysTick->VAL = 0UL; /* Load the SysTick Counter Value */
SysTick->CTRL = SysTick_CTRL_CLKSOURCE_Msk |
SysTick_CTRL_TICKINT_Msk |
SysTick_CTRL_ENABLE_Msk; /* Enable SysTick IRQ and SysTick Timer */
return (0UL); /* Function successful */
}
#endif
/*@} end of CMSIS_Core_SysTickFunctions */
2022-08-31 1:19 AM
It looks like youre writting the setup functions yourself.
Please use Human Readable names for your structs, everyone including you will be happier (maybe OsciInit instead of x0).
My guess is: you got the NVIC stuff wrong.
im just going to take a look at what cubeMX generates (for my stm32f205) and compare it to your code (you should do the same for your stm32f4)
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
Inside HAL_Init i would take a look to what is going on in HAL_InitTick() this may give you some clues.
HAL_StatusTypeDef HAL_Init(void)
{
/* Configure Flash prefetch, Instruction cache, Data cache */
#if (INSTRUCTION_CACHE_ENABLE != 0U)
__HAL_FLASH_INSTRUCTION_CACHE_ENABLE();
#endif /* INSTRUCTION_CACHE_ENABLE */
#if (DATA_CACHE_ENABLE != 0U)
__HAL_FLASH_DATA_CACHE_ENABLE();
#endif /* DATA_CACHE_ENABLE */
#if (PREFETCH_ENABLE != 0U)
__HAL_FLASH_PREFETCH_BUFFER_ENABLE();
#endif /* PREFETCH_ENABLE */
/* Set Interrupt Group Priority */
HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
/* Use systick as time base source and configure 1ms tick (default clock after Reset is HSI) */
HAL_InitTick(TICK_INT_PRIORITY);
/* Init the low level hardware */
HAL_MspInit();
/* Return function status */
return HAL_OK;
}
Then compare your clock initializtion to this(from a stm32f205)
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 240;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 5;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
Error_Handler();
}
}
2022-08-31 1:27 AM
SysTick shouldn't be hard to start properly using standard functions..