H5 1.2.0 and Cube 1.5 break ethernet
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-21 10:59 AM
After updating Cube to v1.5 for my STM32H5 project (Nucleo-H563ZI), the ethernet stopped working except during the initial run after a load of the firmware with the debugger. After a reset, either POR or via the debugger, pings to the board fail. When I checkout an earlier version of the code that uses a Cube v1.4 .ioc file, and bypass the migration to v1.5, the ethernet behaves normally. Has anyone else experienced a similar issue?
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-18 8:53 AM
Hello @robmilne ,
I confirm the issue, I reported the issue internally.
Internal ticket number: 179408. (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-18 8:53 AM
Hello @robmilne ,
I confirm the issue, I reported the issue internally.
Internal ticket number: 179408. (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-18 10:55 AM
Hi STea,
Another issue, that is not a show stopper, is that POR/BOR reset will not allow the LAN8742 to function properly. At the top of my main routine, I inspect the state of the RCC_RSR register and immediately issue a sw reset if it equals the default 0x0c000000 value. Pin or software resets permit the ethernet transceiver to run properly. I had the same issue on one of our prototype boards that uses an ethernet connector with integrated magnetics.
-rob
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-13 9:17 AM
Hello @robmilne ,
can you please share with me the project that caused the Ethernet to Fail with IDE1.15.
regarding the problem with POR/BOR thank you for pointing this out. but I don't seem to see this kind of behavior on Nucleo boards.
BR
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-25 10:17 AM
Hello @robmilne!
Please look at https://community.st.com/t5/stm32-mcus-embedded-software/netxduo-not-working-with-a-static-ip-addresss/td-p/673975. Seems to be similar to what you're facing.
Please let me know if that solution works for you.
BR,
FabioFly
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-05-27 6:12 AM
Hi FabioFly,
If you use Vin as rgw power source (JP2 to to 'VIN 5V'), it does not work on POR/BOR. It works with a reset source of RCC_RSR_PINRSTF or RCC_RSR_SFTRSTF (I haven't checked WDG resets).
I can get it to work if I monitor the reset source at the start of main. The following is what I need to do to get it working.
/* USER CODE BEGIN PTD */
typedef enum reset_e {
RCC_RESET_POR_BOR = 0, /*!< POR or BOR reset occurred (default) */
RCC_RESET_PIN, /*!< Reset from pin occurred */
RCC_RESET_SOFTWARE, /*!< system reset generated by the CPU */
RCC_RESET_WWDG, /*!< window watchdog reset occurred from WWDG */
RCC_RESET_IWDG, /*!< independent watchdog reset occurred */
RCC_ILLEGAL_STOP_ENTRY, /*!< Illegal low-power mode reset occurred */
RCC_RESET_UNKNOWN
} reset_t;
/* USER CODE END PTD */
/* USER CODE BEGIN 0 */
reset_t getReset(void)
{
/* HAL_RCC_GetResetSource() resets interrupt flags in RCC_RSR register */
uint32_t reset_src=HAL_RCC_GetResetSource();
if ((RCC_RSR_PINRSTF) == reset_src) {
return RCC_RESET_PIN;
}
if ((RCC_RSR_PINRSTF | RCC_RSR_BORRSTF) == reset_src) {
return RCC_RESET_POR_BOR;
}
if ((RCC_RSR_PINRSTF | RCC_RSR_SFTRSTF) == reset_src) {
return RCC_RESET_SOFTWARE;
}
if ((RCC_RSR_PINRSTF | RCC_RSR_WWDGRSTF) == reset_src) {
return RCC_RESET_WWDG;
}
if ((RCC_RSR_PINRSTF | RCC_RSR_IWDGRSTF) == reset_src) {
return RCC_RESET_IWDG;
}
if ((RCC_RSR_PINRSTF | RCC_RSR_LPWRRSTF) == reset_src) {
return RCC_ILLEGAL_STOP_ENTRY;
}
return RCC_RESET_UNKNOWN;
}
/* USER CODE END 0 */
int main(void)
{
/* USER CODE BEGIN 1 */
reset_t reset = getReset();
if (RCC_RESET_POR_BOR == reset)
{
volatile int i;
for (i = 0; i < 0x400000; i++) {};
HAL_NVIC_SystemReset();
}
...
/* USER CODE END 1 */
-rob