2023-11-30 10:58 PM
Is it possible to disable a specific GPIO interrupt in my code and re-enable it after some time. HAL_NVIC_DisableIRQ(EXTI4_15_IRQn) this function will help but this will disable all the GPIO pins connected to that particular EXTI line. Any other possible ways I can implement?
Solved! Go to Solution.
2023-12-01 12:08 PM
2023-11-30 11:16 PM
Which STM32?
In most STM32 the individual EXTI interrupts are enabled/disabled in the EXTI_IMR register, see EXTI chapter in Reference Manual (RM).
JW
2023-12-01 01:13 AM - edited 2023-12-01 01:13 AM
I am using STM32G474RCT6 controller.
Should I need to make changes in the EXTI_IMR register. Or are there any HAL functions I can use to Implement this. Currently I could be able to disable EXTI15_10_IRQn which disables all the GPIOs connected to this line.
2023-12-01 02:01 AM
I don't use Cube/HAL.
I've seen in the past users to perform the same operation as when initializing the pin, just without the interrupt being set.
JW
2023-12-01 02:31 AM
Hello @Sri_Nishanth
According to the reference manual, EXTI line dedicated to 10->15 are regrouped in one vector in NVIC controller. So, using CMSIS, this should not be possible. Maybe, we can implement this operation in HAL driver using directly EXTI_IMR. I will forward the request to dedicated team.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-12-01 03:08 AM
2023-12-01 12:08 PM
You can use LL_EXTI_EnableIT_0_31() and LL_EXTI_DisableIT_0_31()
2023-12-03 09:20 PM
Thanks!!
This worked😀🤝