cancel
Showing results for 
Search instead for 
Did you mean: 

GPIO HAL Sanity Check

Carl_G
Senior

I need a second pair of eyes. I am trying to setup EXTI using the GPIO HAL. But it looks like its doing it wrong. It must be me but I need you to double check to be sure.

This is STM32G0 HAL so stm32g0xx_hal_gpio.c

 

/*--------------------- EXTI Mode Configuration ------------------------*/
      /* Configure the External Interrupt or event for the current IO */
      if ((GPIO_Init->Mode & EXTI_MODE) != 0x00u)
      {
        temp = EXTI->EXTICR[position >> 2u];
        temp &= ~(0x0FuL << (8u * (position & 0x03u)));
        temp |= (GPIO_GET_INDEX(GPIOx) << (8u * (position & 0x03u)));
        EXTI->EXTICR[position >> 2u] = temp;

 

 

In this code sample the macro GPIO_GET_INDEX is used. It takes the value "GPIO_TypeDef *GPIOx" and this value will enter the function as  GPIOB, GPIOA etc. The macro is 

 

#if defined(GPIOE)   
#define GPIO_GET_INDEX(__GPIOx__)    (((__GPIOx__) == (GPIOA))? 0uL :\
                                      ((__GPIOx__) == (GPIOB))? 1uL :\
                                      ((__GPIOx__) == (GPIOC))? 2uL :\
                                      ((__GPIOx__) == (GPIOD))? 3uL :\
                                      ((__GPIOx__) == (GPIOE))? 4uL : 5uL)
#else
#define GPIO_GET_INDEX(__GPIOx__)    (((__GPIOx__) == (GPIOA))? 0uL :\
                                      ((__GPIOx__) == (GPIOB))? 1uL :\
                                      ((__GPIOx__) == (GPIOC))? 2uL :\
                                      ((__GPIOx__) == (GPIOD))? 3uL : 5uL)
#endif /* GPIOE */

 

There is no GPIOE so the second macro. The problem is if you pass in GPIOA you get a 0. 0s don't shift. So the statement 

temp |= (GPIO_GET_INDEX(GPIOx) << (8u * (position & 0x03u)));

Will always result in a 0 for GPIOA. Which means EXTI is never setup for GPIOA. But even worse, GPIOB is also 1 position off. It seems this statement requires something indexed to 1 and not to 0. It is the result I am getting in my software. EXTI is not being setup correctly when I do this.

Am I misreading it??

1 ACCEPTED SOLUTION

Accepted Solutions

> Why even care about the previous value if its not bitwise?

I don't know what do you mean by "bitwise" here, but for example, let's assume you have EXTI0 set previously to  PB0 (and the rest of EXTIs are left at their reset value), i.e. EXTI_EXTICR1=0x01. Now if you want to change the setting of EXTI0 to PC0, you would need to change EXTI_EXTICR1 to 0x02, but unless you clear the lowermost 8 bits of EXTI_EXTICR1, just by ORing 0x02 to it, you would set it to 0x03, which is not what you want.

> So either PA6 or PB6 or PC6 but only one of them. No one has ever mentioned this in their lessons or videos...

Again I don't know what are the "lessons and videos" you are mentioning here, but if they don't mention this fact, well that's unfortunate and maybe not quite right, but then, "lessons and videos" are not the primary information source, the RM is. And, as witnessed by your own remark, the RM is pretty clear in this regard.

JW

View solution in original post

7 REPLIES 7
TDK
Guru

GPIOA is selected when the field is zero, GPIOB is 1, etc. The statement before clears the field. Seems correct. Look at the description of exticr in the reference manual.

If you feel a post has answered your question, please click "Accept as Solution".
Carl_G
Senior
Spoiler
 

I guess i was confused because the reference manual says "these bits are written" implying its bitwise. But with PD being 3 it can't be bitwise.  This implies only one of any given numbered port can trigger an interrupt or be a wakeup. So either PA6 or PB6 or PC6 but only one of them. No one has ever mentioned this in their lessons or videos...

 

This is a bit strange though isn't it? If its not bitwise why the &=~ and the |=  Why even care about the previous value if its not bitwise?

> Why even care about the previous value if its not bitwise?

I don't know what do you mean by "bitwise" here, but for example, let's assume you have EXTI0 set previously to  PB0 (and the rest of EXTIs are left at their reset value), i.e. EXTI_EXTICR1=0x01. Now if you want to change the setting of EXTI0 to PC0, you would need to change EXTI_EXTICR1 to 0x02, but unless you clear the lowermost 8 bits of EXTI_EXTICR1, just by ORing 0x02 to it, you would set it to 0x03, which is not what you want.

> So either PA6 or PB6 or PC6 but only one of them. No one has ever mentioned this in their lessons or videos...

Again I don't know what are the "lessons and videos" you are mentioning here, but if they don't mention this fact, well that's unfortunate and maybe not quite right, but then, "lessons and videos" are not the primary information source, the RM is. And, as witnessed by your own remark, the RM is pretty clear in this regard.

JW

Carl_G
Senior

I see it now. The bitwise operations are because there are 4 different EXTI in each register. When changing one of them you still need to maintain the other 3.

EXTI registers are byte-wise accessible, so you can write something like, for example,

((volatile uint8_t*)&EXTI->EXTICR[0])[3] = 1;

to set PB3 as EXTI3 source.

JW

Interesting. I wonder why the HAL writers didn't employ this feature. Would have made the code much easier. But also would have been confusing.

This arrangement is relatively new. The EXTI GPIO mux selector used to be in SYSCFG, not bytewise-accessible, and the fields used to be 4-bits wide.

JW