getting BSP_ERROR_CLOCK_FAILURE from BSP_AUDIO_IN_Init().
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-06-30 10:28 PM
Hi All,
I have a B-U585I-IOT02A board and the freeRTOS is flashed
- https://github.com/FreeRTOS/iot-reference-stm32u5
It has 2 digital microphones, but /iot-reference-stm32u5 does not include the BSP for audio.
So I merged the audio BSP from STM32CubeU5 MCU Firmware Package.
The building is done but I'm getting an error (BSP_ERROR_CLOCK_FAILURE) from BSP_AUDIO_IN_Init().
/**
BSP_AUDIO_Init_t AudioInit;
gAudio.Instance = 0;
AudioInit.Device = AUDIO_IN_DEVICE_DIGITAL_MIC1;
AudioInit.SampleRate = AUDIO_FREQUENCY_11K;
AudioInit.BitsPerSample = AUDIO_RESOLUTION_16B;
AudioInit.ChannelsNbr = 1;
AudioInit.Volume = 100;
status = BSP_AUDIO_IN_Init(gAudio.Instance, &AudioInit);
**/
Finally, RCCEx_PLL3_Config9) returned "HAL_TIMEOUT"
/**
static HAL_StatusTypeDef RCCEx_PLL3_Config(RCC_PLL3InitTypeDef *pll3)
{
......
/* Wait till PLL3 is ready */
while (__HAL_RCC_GET_FLAG(RCC_FLAG_PLL3RDY) == 0U)
{
if ((HAL_GetTick() - tickstart) > PLL3_TIMEOUT_VALUE)
{
return HAL_TIMEOUT;
}
}
return HAL_OK;
}
**/
How to resolve it?
- Labels:
-
Audio
-
STM32U5 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-08-10 05:53 PM
Hello,
Could you refer to the setting of the following project ~\Projects\B-U585I-IOT02A\Examples\BSP from the STM32CubeU5 FW.
The RCC_FLAG_PLL3RDY is set by HW when the PLL3 is ready, so try to compare your setting versus the one in project provided by STM32U5Cube.
Be sure also that the MDF/ADF peripherals filters are properly activated.
Best regards,
Younes