2025-11-25 12:55 AM - last edited on 2025-11-25 1:48 AM by Andrew Neil
Hi there.
I’m trying to generate a 12 ns pulse for a time-of-flight (ToF) application.
I’m using an STM32U5 microcontroller, and I’d like to know whether one of the general-purpose timers (TIM2/TIM3/TIM4/TIM5) can produce a pulse that narrow. With a 160 MHz timer clock, the time resolution is about 6 ns, so in principle it seems feasible, but I may be overlooking something.
Thanks!
Solved! Go to Solution.
2025-11-26 3:36 AM
In the end, I realized I hadn’t been interpreting my results correctly. The pulse shown earlier in IMG_0794 was actually inverted, the relevant pulse was the low portion, not the high one. This means the pulse width was around 200 ticks.
This behavior occurs because, in the selected PWM mode combined with one-pulse mode, the output goes low when the counter transitions from TIMx_CCR to TIMx_ARR. Therefore, for example, if we want a 2-tick low pulse, setting CCR = 198 and ARR = 200 should produce the expected result.
Sorry for the confusion, and thanks to everyone for the support.
Cheers!
2025-11-25 1:27 AM
hello @lucascalam
To generate a pulse of about 12 ns using an STM32U5 timer running at 160 MHz, you can:
This will produce a pulse very close to 12 ns directly from the timer hardware without CPU intervention.
2025-11-25 1:33 AM
Hi @T_Hamdi , thanks a lot for your answer. Do you know if there is any example I can use as a guide?
2025-11-25 1:38 AM
> This will produce a pulse very close to 12 ns directly from the timer hardware without CPU intervention.
This time would correspond to 2 single-cycle (pipelined) core instructions.
In other words, this is not achievable by the core itself.
Another option would be external hardware.
2025-11-25 2:07 AM
hello @Ozone
using the STM32U5 timer hardware running at 160 MHz, you can generate a pulse of approximately 12.5 ns (2 timer ticks) via PWM or Output Compare mode without CPU intervention. This is achievable because the timer operates independently of the CPU pipeline.
2025-11-25 2:32 AM
Yes, I understood that.
My point is, there is no alternative based upon core performance alone.
2025-11-25 5:42 AM
I am using something like this:
void WHGPIO_PinOutSendPulse1(void) {
LL_TIM_EnableCounter(TIM2);
}
void WHGPIO_InitPinOutSendPulse(void) {
LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOA);
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_TIM2);
LL_GPIO_InitTypeDef gpio_init = {0};
gpio_init.Pin = LL_GPIO_PIN_1;
gpio_init.Mode = LL_GPIO_MODE_ALTERNATE;
gpio_init.Alternate = LL_GPIO_AF_1; // TIM2_CH2 → AF1 on PA1
gpio_init.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
gpio_init.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
gpio_init.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(GPIOA, &gpio_init);
LL_TIM_DisableCounter(TIM2);
LL_TIM_OC_SetPolarity(TIM2, LL_TIM_CHANNEL_CH2, LL_TIM_OCPOLARITY_HIGH);
LL_TIM_SetPrescaler(TIM2, 0);
LL_TIM_SetAutoReload(TIM2, 200);
LL_TIM_OC_SetCompareCH2(TIM2, 1);
LL_TIM_OC_SetMode(TIM2, LL_TIM_CHANNEL_CH2, LL_TIM_OCMODE_PWM1);
LL_TIM_OC_EnablePreload(TIM2, LL_TIM_CHANNEL_CH2);
LL_TIM_EnableARRPreload(TIM2);
LL_TIM_SetOnePulseMode(TIM2, LL_TIM_ONEPULSEMODE_SINGLE);
LL_TIM_CC_EnableChannel(TIM2, LL_TIM_CHANNEL_CH2);
LL_TIM_GenerateEvent_UPDATE(TIM2);
}
void main() {
WHGPIO_InitPinOutSendPulse();
while(1) {
WHGPIO_PinOutSendPulse1();
}
}I obtained the results shown in the attached images. From the first graph, we can see that the pulse width is significantly larger than 12 ns. The second graph shows the interval between pulses, which is about 1.25 µs. This is expected, since the auto-reload value is set to 200 ticks, and 200 × 6.25 ns = 1.25 µs. So, while the frequency appears to be configured correctly, the pulse width does not.
2025-11-25 6:04 AM
hello @lucascalam
To achieve a pulse width of approximately 12 ns, you need to increase the compare value in your code from:
LL_TIM_OC_SetCompareCH2(TIM2, 2);
each timer tick corresponds to about 6.25 ns at 160 MHz, setting the compare register to 2 will produce a pulse width close to 12.5 ns, effectively doubling the pulse duration from 6.25 ns to approximately 12 ns.
2025-11-25 6:09 AM
hello @T_Hamdi .
Thanks for your answer. The problem is that even when the compare value is set to 1, the pulse width that I get is more than 50ns, as the image that I attached on the previous reply. Do you have any idea why the pulse is always longer than the expected 6ns (or 12ns in case the compare value is set to 2 ticks) ?
2025-11-25 6:16 AM
hello @lucascalam
To understand why your pulse width is longer than expected, you should first check the actual timer clock frequency. If the timer runs at a lower frequency than 160 MHz, each timer tick will be longer, which increases the pulse width.