2014-12-03 1:44 PM
g
#hal_uart_error_pe-uart-parity2014-12-04 8:50 AM
Please don't do that, it damages the integrity of the forum
''Hi
I am using STM32F407 micro to implement UART communication with two HW modules using UART4 and UART5.
I used CUBE Mx to generate my code one of them is configures with 9 data bits and one parity bit ,send and receive in interrupt mode while the other is configured 8 data bits and no parity bits , send in polling mode and receive in interrupt mode
The Problem is That I a parity Error handler called from the 8data bits ISR?
IS that normal?, How can I avoid such problem?
Salam
Hossam Alzomor''
2014-12-04 10:20 AM
Hi Clive,
I sent the post and the next day I discovered the cause of the problem, while my description of it was not accurate, I tried to remove the post but couldn't find a method on the forum to remove the post. I removed the body body of the message and expected that will remove the whole message.2014-12-09 2:38 AM
Hi Hossam,
I agree with Clive1.The recommended practice is to edit or add a new post saying that the problem was resolved & if possible also tell other forum users what was the solution. This will be more helpful & very appreciated.Welcome on our community!-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.