2023-03-14 4:17 AM
I'm trying to build a project using FileX in standalone mode (without ThreadX dependecies). According to Microsoft's documentation the FX_STANDALONE_ENABLE flag must be defined in order to disable the use of ThreadX specifics (timers, semaphores etc.), but I can't seem to find this option in CubeMX when generating code. I've noticed that the documentation by Microsoft is deprecated in some areas (in regards to function names for instance), and am wondering if this flag might have been replaced by some other flag or if there is another way to run FileX in standalone mode?
Solved! Go to Solution.
2023-03-14 6:00 AM
Hi @Hermund Døssland , Can you please update the version of X-CUBE-AZRTOS-H7 to 3.0.0 it support USBX and FileX without RTOS. if you download the package from ST.com you can find the IOC of Fx_File_Edit_Standalone application.
https://www.st.com/en/embedded-software/x-cube-azrtos-h7.html
you can refer to this application :
2023-03-14 6:00 AM
Hi @Hermund Døssland , Can you please update the version of X-CUBE-AZRTOS-H7 to 3.0.0 it support USBX and FileX without RTOS. if you download the package from ST.com you can find the IOC of Fx_File_Edit_Standalone application.
https://www.st.com/en/embedded-software/x-cube-azrtos-h7.html
you can refer to this application :
2023-09-04 1:21 AM
There is no IOC file in this folder, please clarify,
I could not find it in the F4 either: