cancel
Showing results for 
Search instead for 
Did you mean: 

Flash Erase not Working (STM32G491RC)

BAdmi.1
Associate II

I'm trying to write some data to a address in the flash memory of the above mentioned chip. However the Erase doesn't seem to work.

 

void writeToFlash(uint32_t address, uint64_t data, uint64_t data2){ // Unlock the Flash Program controller HAL_FLASH_Unlock(); // Setting Up the Erase FLASH_EraseInitTypeDef EraseInitStruct; EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES; EraseInitStruct.Banks = 2; EraseInitStruct.Page = 127; EraseInitStruct.NbPages = 1; // simple function only sending 8 Bytes at the time. uint32_t pageError; //Erasing specific part of memory HAL_FLASHEx_Erase(&EraseInitStruct, &pageError); //Programming the flash, last adress of the second Bank! HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, address, data); HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, address + 0x08, data2); //Locking the flash back up HAL_FLASH_Lock(); }

 

In the main I'm calling the following:

 

writeToFlash(0x0807FFF0, 0x00FFFFFF9A6410AC, 0x00000000016410AC);

 

The reason I'm specifying the bank and page number is because I (think I,) know where the data needs to be erased.

And when do a full chip erase via STM32Cube Programmer, the writing to the flash works. But when I try to do it with some data storage already in the memory. It doesn't. Please help, I've been struggling now for a couple of days.

Capture.PNG

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
GwenoleB
ST Employee

Hello @BAdmi.1,

You are using a G491RC with 256KBytes of Flash size in single bank only.

Dual bank is supported on devices STM32G4x3 Series.

Best Regards,

Gwénolé

 

View solution in original post

4 REPLIES 4

Try just erasing in the program, nothing else; and then read out the erased area using CubeProgrammer - was it erased?

JW

Not when i try it in the second bank, when i run the program for the last page of the first bank. It works just fine:

void writeToFlash(uint32_t address, uint64_t data, uint64_t data2){ // Unlock the Flash Program controller HAL_FLASH_Unlock(); // Setting Up the Erase FLASH_EraseInitTypeDef EraseInitStruct; EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES; EraseInitStruct.Banks = 0x01; EraseInitStruct.Page = 126; EraseInitStruct.NbPages = 2; // simple function only sending 8 Bytes at the time. uint32_t pageError; //Erasing specific part of memory HAL_FLASHEx_Erase(&EraseInitStruct, &pageError); //Programming the flash, last adress of the second Bank! HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, address, data); HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, address + 0x08, data2); //Locking the flash back up HAL_FLASH_Lock(); }

And calling it with:

writeToFlash(0x0803FFF0, 0x00FFFFFF9A6410AC, 0x00000000016410AC); // and to test wheter i can change it writeToFlash(0x0803FFF0, 0x00FFFFFF906410AC, 0x00000000016410AC); // the data i write btw corresponds to IP adresses that have to be looked up after restarting

BAdmi1_1-1704285146658.png

BAdmi1_2-1704285204115.png

BAdmi1_3-1704285232278.png

So my code works when i try it in the first bank, when i try it in the second bank it fails.
Changing banks value to 0x02 doesn't work. But why?

I don't use Cube/HAL, but it's open source, so you can debug it as usually: observe what is written to the FLASH registers, and compare it against the description in Reference Manual.

JW

GwenoleB
ST Employee

Hello @BAdmi.1,

You are using a G491RC with 256KBytes of Flash size in single bank only.

Dual bank is supported on devices STM32G4x3 Series.

Best Regards,

Gwénolé