2020-04-24 11:25 PM
I worked on ethernet in NUCLEO-H743ZI2 and it was working properly. But when I developed my own PCB and used the same ethernet circuit as nucleo board, ethernet connection is not even detected.
2020-04-26 12:57 PM
With such a "detailed" description it's impossible to help.
Also take a note of these...
https://community.st.com/s/question/0D50X0000C6eNNSSQ2/bug-fixes-stm32h7-ethernet
2020-05-29 02:38 AM
It worked after I pulled down the LED2 pin to gnd through 10k resistor.
2020-05-30 03:39 AM
> the same ethernet circuit as nucleo board
Well, then this was a lie and a good lesson to read the datasheet.