cancel
Showing results for 
Search instead for 
Did you mean: 

Driver Support for Video Class for USB .

KRaj.1
Associate

Hi ,

This is Krishnaraj K , Project Associate , CEET, IITMRP . We are in need to interface C270 USB Webcam Interface with Stm32l496Ret6 Microcontroller . We found a source at which is wriiten for stm32f429zi . But its difficult to migrate to our microcontroller .Would be fine if there any official Driver for UVC . Awating for good response .

Thanks

Krishnaraj K

krishnarajk@tenet.res.in

5 REPLIES 5
mohamed.ayed
ST Employee

Hi @Krishna Raj​ ,

welcome to our community :smiling_face_with_smiling_eyes:.

You can use USBX Middleware it support UVC host class, Unfortunately we don't have until yet Video Host example or template in our packages

Waiting for that delivery, you may use Microsoft Azure RTOS documentation in order to develop your own application.

See also: https://github.com/azure-rtos/usbx/issues/4

you can download x-cube-azrtos-l4 pack from CubeMx configure and generate your project.

Best Regards,

Mohamed

Hi @mohamed.ayed​ 

Thanks for your Suggestion . I will look into that and revert back !

Best Regards

Krishna

pankaj19
Associate

Hii @KRaj.1 

This is Pankaj Padhiyar , under graduate student at charusat university . I want to know more about interfacing C270 USB Webcam to stm32 peripheral board ,can you give me more idea about that , My project is about image processing using stm32 nucleof767zi peripheral board .

Thanks

Pankaj Padhiyar

21EC025@charusat.edu.in

Are there any updates on this? 

I am trying to use a webcam using STM32H723 on a custom setup. I have successfully setup USBx and ThreadX libraries. For some reason, the MCU is not able to recognize camera connection. 

Pavel A.
Evangelist III

While waiting for more satisfying responses, try to find help here and set your project rolling now.