cancel
Showing results for 
Search instead for 
Did you mean: 

does anybody have source code for LG4571 display (480 x 800)

MNapi
Senior III

there is nothing on  github.

 

there is initialization by SPI before the LTDC works

is there a sequence like you initialize it first over SPI then

MX_LTDC_Init() or it does not matter

I do have the initialization code but I am missing something

void SLGDP4571_Int(void)
{

SPI_WriteComm(0x20);

SPI_WriteComm(0x3A);
SPI_WriteData(0x70);

SPI_WriteComm(0xB1);
SPI_WriteData(0x10);
SPI_WriteData(0x14);
SPI_WriteData(0x06);

SPI_WriteComm(0xB2);
SPI_WriteData(0x00);
SPI_WriteData(0xC8);

SPI_WriteComm(0xB3);
SPI_WriteData(0x11);
SPI_WriteData(0xFF);

SPI_WriteComm(0xB4);
SPI_WriteData(0x10);

SPI_WriteComm(0xB6);
SPI_WriteData(0x08);
SPI_WriteData(0x18);
SPI_WriteData(0x02);
SPI_WriteData(0x40);
SPI_WriteData(0x10);

SPI_WriteComm(0xB7);
SPI_WriteData(0x00);
SPI_WriteData(0x10);
SPI_WriteData(0x01);

SPI_WriteComm(0xC3);
SPI_WriteData(0x04);
SPI_WriteData(0x05);
SPI_WriteData(0x04);
SPI_WriteData(0x04);
SPI_WriteData(0x01);

SPI_WriteComm(0xC4);
SPI_WriteData(0x22);
SPI_WriteData(0x03);
SPI_WriteData(0x00);
SPI_WriteData(0x1A);
SPI_WriteData(0x1A);
SPI_WriteData(0x05);
SPI_WriteData(0x00);
SPI_WriteData(0x04);

SPI_WriteComm(0xC5);
SPI_WriteData(0x6C);

SPI_WriteComm(0xC6);
SPI_WriteData(0x23);
/****
SPI_WriteComm(0xC8);
SPI_WriteData(0x01);
SPI_WriteData(0x01);
SPI_WriteData(0x03);
SPI_WriteData(0xFF);
***/

SPI_WriteComm(0xD0);
SPI_WriteData(0x00);
SPI_WriteData(0x43);
SPI_WriteData(0x64);
SPI_WriteData(0x25);
SPI_WriteData(0x10);
SPI_WriteData(0x02);
SPI_WriteData(0x71);
SPI_WriteData(0x44);
SPI_WriteData(0x04);

SPI_WriteComm(0xD1);
SPI_WriteData(0x00);
SPI_WriteData(0x43);
SPI_WriteData(0x64);
SPI_WriteData(0x25);
SPI_WriteData(0x10);
SPI_WriteData(0x02);
SPI_WriteData(0x71);
SPI_WriteData(0x44);
SPI_WriteData(0x04);

SPI_WriteComm(0xD2);
SPI_WriteData(0x00);
SPI_WriteData(0x43);
SPI_WriteData(0x64);
SPI_WriteData(0x25);
SPI_WriteData(0x10);
SPI_WriteData(0x02);
SPI_WriteData(0x71);
SPI_WriteData(0x44);
SPI_WriteData(0x04);

SPI_WriteComm(0xD3);
SPI_WriteData(0x00);
SPI_WriteData(0x43);
SPI_WriteData(0x64);
SPI_WriteData(0x25);
SPI_WriteData(0x10);
SPI_WriteData(0x02);
SPI_WriteData(0x71);
SPI_WriteData(0x44);
SPI_WriteData(0x04);

SPI_WriteComm(0xC2);
SPI_WriteData(0x08);
HAL_Delay(20);
SPI_WriteComm(0xC2);
SPI_WriteData(0x18);
HAL_Delay(20);
SPI_WriteComm(0xC2);
SPI_WriteData(0xB8);
HAL_Delay(20);
SPI_WriteComm(0xB5);
SPI_WriteData(0x01);
HAL_Delay(20);
SPI_WriteComm(0x29);
HAL_Delay(20);

}

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
MNapi
Senior III

This is not the first time I am having problem to send data over SPI, that was the problem again.

You would have to see on logic analyzer to compare the waves.

So I disabled SPI and assigned PINs as output. And I made my own SPI interface using pins as output. And it worked fine, the display is initializing and working.

 

void SPI_SendData(unsigned char i)
{
unsigned char n;

for(n=0; n<8; n++)
{
if(i&0x80) HAL_GPIO_WritePin(GPIOI, GPIO_PIN_3, GPIO_PIN_SET);
else HAL_GPIO_WritePin(GPIOI, GPIO_PIN_3, GPIO_PIN_RESET);
i<<= 1;

HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);//_nop_(); _nop_();_nop_();_nop_();

HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_SET);//_nop_();_nop_();_nop_();_nop_();

}
}

 

If somebody has similar problem with initialization over SPI does not work that might be the solution.

Maybe somebody from STM can collaborate?

View solution in original post

4 REPLIES 4
SofLit
ST Employee

Hello @MNapi ,

Please use </> button to share your code.. I've edited your post then.. 

Please refer to the tips on how to post a thread.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
MNapi
Senior III

This is not the first time I am having problem to send data over SPI, that was the problem again.

You would have to see on logic analyzer to compare the waves.

So I disabled SPI and assigned PINs as output. And I made my own SPI interface using pins as output. And it worked fine, the display is initializing and working.

 

void SPI_SendData(unsigned char i)
{
unsigned char n;

for(n=0; n<8; n++)
{
if(i&0x80) HAL_GPIO_WritePin(GPIOI, GPIO_PIN_3, GPIO_PIN_SET);
else HAL_GPIO_WritePin(GPIOI, GPIO_PIN_3, GPIO_PIN_RESET);
i<<= 1;

HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);//_nop_(); _nop_();_nop_();_nop_();

HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_SET);//_nop_();_nop_();_nop_();_nop_();

}
}

 

If somebody has similar problem with initialization over SPI does not work that might be the solution.

Maybe somebody from STM can collaborate?

>>Maybe somebody from STM can collaborate?

Work with your account's FAE (support enginer), or other engineers on your team.

>>If somebody has similar problem with initialization over SPI does not work that might be the solution.

Probably timing or edge/phase configuration issues.

Check controller data sheet about expectations for CS, and data timing expectations.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

This is how it looks now

display.jpg