cancel
Showing results for 
Search instead for 
Did you mean: 

Do I need an external crystal if I want to use the STM32F412 USB FS device ? or can I use the internal HSI ?

EFish.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
9 REPLIES 9
berendi
Principal

Yes, the internal oscillator can not provide the accuracy required by USB.

frank.zhao
Associate II

STM32 chips with crystal-less USB are

STM32F072

STM32F078

STM32F04x

STM32F105/107

STM32H743/753

STM32H750

STM32L0x2

STM32L0x3

STM32L4x2

STM32L4x3

STM32L4x5

STM32L4x6

STM32L4Rx

STM32L4Sx

waclawek.jan
Super User

I wonder how would 'F105/107 work crystal-less. Can you please post source?

JW

@Community member​ I'm reading AN4879 "USB implementation on STM32 products", section 2.1, table 4 "USB implementation on STM32 mainstream products". F105/107 does indeed have a X under crystal-less. But reading the datasheet I can't see that feature.

waclawek.jan
Super User

@Imen DAHMEN​  Hi, this appears to be an error, can you please have a look at it?

Thanks,

Jan

S.Ma
Principal

To complement: Most STM32L4 have MSI which generates 48MHz from the 32.768kHz LSE and is suitable for USB Device function without LSE.

In Host mode, HSE crystal becomes required.

The G4 series also has crystal-less USB using the CRS.

Ok, I will check and raise it internally for fix.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Thanks, Imen.

JW