cancel
Showing results for 
Search instead for 
Did you mean: 

DMA -> MDMA chaining stm32h7

MonsieurShann
Associate II

Hello everyone,

Context

I am having troubles chaining the DMA1 and MDMA of the stm32h755, more precisely, I am looking for the following data flow when reading data from SPI, the SPI being regularly triggered  : 

SPI -> DMA1 Channel3 -> SRAM -> MDMA Channel 3 -> DTCM.

I transfer 4 halfwords between my SPI and my SRAM. I also want to move 4 halfwords between my SRAM and my DTCM thanks to the MDMA.

The connection between the DMA1 Channel 3 and the MDMA Channel 3 being the DMA1 Channel Transfer complete request.

Problem

I have no problem moving data from SPI to SRAM using DMA1 Channel 3 every time I read something on my SPI.
However my MDMA is only working on the first transfer, then he's not transfering no more, even if my DMA1 Channel 3 transfer complete has triggered. I could not figure why..

Code : 

 

hmdma_mdma_channel3_dma1_stream3_tc_0.Instance = MDMA_Channel3; hmdma_mdma_channel3_dma1_stream3_tc_0.Init.Request = MDMA_REQUEST_DMA1_Stream3_TC; // Requête déclenchée par DMA1_Stream3_TC hmdma_mdma_channel3_dma1_stream3_tc_0.Init.TransferTriggerMode = MDMA_BUFFER_TRANSFER; hmdma_mdma_channel3_dma1_stream3_tc_0.Init.Priority = MDMA_PRIORITY_LOW; hmdma_mdma_channel3_dma1_stream3_tc_0.Init.Endianness = MDMA_LITTLE_ENDIANNESS_PRESERVE; hmdma_mdma_channel3_dma1_stream3_tc_0.Init.SourceInc = MDMA_SRC_INC_HALFWORD; // Incrémentation de la source hmdma_mdma_channel3_dma1_stream3_tc_0.Init.DestinationInc = MDMA_DEST_INC_HALFWORD; // Incrémentation de la destination hmdma_mdma_channel3_dma1_stream3_tc_0.Init.SourceDataSize = MDMA_SRC_DATASIZE_HALFWORD; hmdma_mdma_channel3_dma1_stream3_tc_0.Init.DestDataSize = MDMA_DEST_DATASIZE_HALFWORD; hmdma_mdma_channel3_dma1_stream3_tc_0.Init.BufferTransferLength = 4; // Transfert de 4 HALFWORDS hmdma_mdma_channel3_dma1_stream3_tc_0.Init.SourceBurst = MDMA_SOURCE_BURST_4BEATS; // Burst de 4 HALFWORDS hmdma_mdma_channel3_dma1_stream3_tc_0.Init.DestBurst = MDMA_DEST_BURST_4BEATS; // Burst de 4 HALFWORDS hmdma_mdma_channel3_dma1_stream3_tc_0.Init.SourceBlockAddressOffset = 0; hmdma_mdma_channel3_dma1_stream3_tc_0.Init.DestBlockAddressOffset = 0;

 

And :

 

HAL_MDMA_Start_IT(&hmdma_mdma_channel3_dma1_stream3_tc_0, (uint32_t)adc_burst_sram, (uint32_t)adc_burst_dtcm, sizeof(adc_burst_sram), 1)

 

If someone has an idea :)

Regards,

1 REPLY 1
Saket_Om
ST Employee

Hello @MonsieurShann 

Please refer to the example Projects/NUCLEO-H7A3ZI-Q/Examples/MDMA/MDMA_LinkedList to set your MDMA transfer.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om