2016-05-05 08:52 AM
This program told me that it successfully created a DFU file (from a binary file) in the directory path that I provided, but the DFU file was NOT there!!! Where might it be? Has anyone else had this problem? My destination path is rather long.
EDIT:C:\Windows\System32was where DFU File Manager put my files.Today when experimenting with DfuSe Demo 3.0.4:I clicked the [Choose.. ] button in the ''Upgrade or verify action'' frame,...and there were all my lost *.dfu files that I had TOLD DFU File Manager 3.04 to save in folder;C:\stm32\my\workspace\OfficeAc6_2016.01_Cube1.11.0\F4\discovery\UseHalCdcStandalone\cppMx08_Tim10_USB_F4Disc_Accel_Q\Debug. Using Windoze7 (32bit)(x86).EDIT2:Oh dear!!The .dfu files that appear to be in C:\Windows\System32 are inaccessible. When I drag one of these dfu files to another folder, windows says it does not exist. When I explore folder C:\Windows\System32 with windows explorer,the files are not even listed.What is going on?EDIT3:reverting to version 3.0.2 was the reluctant solution in the end.What would we do without Clive1 making that old version available to us? Thank you Clive1 for that (indirect) linkhttps://drive.google.com/file/d/0B7OY5pub_GfIdTE0N18ycHl2NlE/view?usp=sharing
. #pile-of-poop-version-3.0.4 #feedback-dfu-manager-win7-x86 #4755=posts13x24hours-@4min/post2016-05-05 09:07 AM
I've had it throw errors, and there are threads about that.
https://community.st.com/0D50X00009XkhKJSAZ
Edited: Fixed DEADLINK
2016-05-05 09:25 AM
Thanks Clive1, yes I saw those threads, they seemed to suggest getting an older release.
2016-05-05 10:33 AM
I'm probably pushing much closer to 30000-40000, the forum has melted down several times during my tenure, and my last ID got locked out as my ISP closed down after 20 years, and I can't get to that email address, and ST (Microsoft Sharepoint) can't change email addresses in their system, or at least that's what I'm lead to believe.
2016-05-11 03:01 AM
I have EDITED the original post with a workaround for the problem,
... or not!2016-05-18 03:07 AM
Hi,
Please note that DFU File Manager 3.0.5 is now available in the web. Please try yo download it from .-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.