Creating 2 TCP threads
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-01 07:45 AM
Hi
I am trying to create two TCP threads for my application.these packets are intended to control two VFDs which has two IP addresses(192.168.10.4 and 192.168.10.5) but same port number(502- modbus TCP).I am able to send packets to both the servers simultaneously. the VFDs gives me encoder data embedded in the TCP packets. when i try to capture the encoder data, i found that the data received in the netbuf is getting mixed up . I mean encoder 1 is displayed in encoder2 position in HMI and vice versa. communication to HMI is UDP. i call the udp transmit function in the respective threads itself.i have given seperate names for the netbuf and all the other buffers. i am clearing netbuf in both the threads.looks as if both the threads are trying to write tha same netbuf. how to resolve this issue. is there any problem in doing 2 TCP threads in LWIP. i have given priorities above normal to one thread and normal to the other one. if i comment the netconn_recv of one thread the other thread will work perfectly and i am getting the correct encoder data. whereas if i comment the UDP tranmission to HMI , i can see the data swtching. that's why i assume that the netbuf is getting updated simultaneously. please help. i am stuck with this issue for the last few days
the relevant portions of the code is attached
thanks in advance
RMG
- Labels:
-
Ethernet
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-01 05:10 PM
A lot of those functions return an err_t value which can indicate an error. I'd start with checking for that. Seems like the memory pool is getting okay.
Putting code within a code block makes it much easier to read compared to a picture of code.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-02 07:04 AM
I am attaching the edited code. though i have given names to err_t vales i am not actually using all of them. can i assign memory location for netbuf. even though i have assigned different names for the netbufs in the threads it looks like both the threads updating the same netbuf. i tried netbuf_delete and netbuf_free. but still the issue is there. please help
Main.c
/* Init thread */
osThreadDef(Start, StartThread, osPriorityNormal, 0, configMINIMAL_STACK_SIZE * 4);
osThreadCreate (osThread(Start), NULL);
/* Start scheduler */
osKernelStart();
for( ;; );
}
static void StartThread(void const * argument)
{
/* Create tcp_ip stack thread */
tcpip_init(NULL, NULL);
/* Initialize the LwIP stack */
Netif_Config();
/* Initialize webserver demo */
mm_thread_init();
sp_thread_init();
for( ;; )
{
/* Delete the Init Thread */
osThreadTerminate(NULL);
}
}
SP thread init function
void sp_vfd_init(void)
{
struct netbuf *inbuf_sp;
err_t recv_err_sp;
char* buf_sp;
u16_t buflen_sp;
struct ip4_addr iDestAddr;
struct netconn *conn_sp;
conn_sp = netconn_new(NETCONN_TCP);
IP_ADDR4(&iDestAddr,192,168,10,5);
if ( ERR_OK == netconn_connect(conn_sp, &iDestAddr, 502))
{
netconn_write(conn_sp, data3, 19, NETCONN_COPY);
while ((recv_err_sp = netconn_recv(conn_sp, &inbuf_sp)) == ERR_OK)
{
do{
netbuf_data(inbuf_sp, (void**)&buf_sp, &buflen_sp);
if (buf_sp[5]==0X09 && buflen_sp == 15)
{
netbuf_copy( inbuf_sp,data_buff_sp,inbuf_sp->p->tot_len);
data_buff_sp[inbuf_sp->p->tot_len]='\0';
data_buff_sp[17]= 0x55;
udp_client_send_sp();
}
else
if ( buf_sp[7]==0X10 && buf_sp[9]==0X04 && buf_sp[11]==0X03 && buflen_sp == 0X0C)
{
netconn_write(conn_sp, data4, 12, NETCONN_COPY);
}
netconn_write(conn_sp, data3, 19, NETCONN_COPY);
vTaskDelay (10);
}while (netbuf_next(inbuf_sp) >= 0);
netbuf_delete(inbuf_sp);
}
}
netconn_close(conn_sp);
netconn_delete(conn_sp);
}
////Second thread function
void mm_vfd_init(void)
{
struct netbuf *inbuf_mm;
err_t recv_err_mm;
char* buf_mm;
u16_t buflen_mm;
struct ip4_addr iDestAddr;
struct netconn *conn_mm;
conn_mm = netconn_new(NETCONN_TCP);
IP_ADDR4(&iDestAddr,192,168,10,4);
if ( ERR_OK == netconn_connect(conn_mm, &iDestAddr, 502))
{
netconn_write(conn_mm, data6, 19, NETCONN_COPY);
while ((recv_err_mm = netconn_recv(conn_mm, &inbuf_mm)) == ERR_OK)
{
do{
netbuf_data(inbuf_mm, (void**)&buf_mm, &buflen_mm);
if (buf_mm[5]==0X09 && buflen_mm == 15)
{
netbuf_copy( inbuf_mm,data_buff_mm,inbuf_mm->p->tot_len);
data_buff_mm[inbuf_mm->p->tot_len]='\0';
data_buff_mm[17]= 0x44;
udp_client_send_mm();
}
else
if ( buf_mm[7]==0X10 && buf_mm[9]==0X04 && buf_mm[11]==0X03 && buflen_mm == 0X0C)
{
netconn_write(conn_mm, data4, 12, NETCONN_COPY);
}
netconn_write(conn_mm, data6, 19, NETCONN_COPY);
vTaskDelay (10);
}while (netbuf_next(inbuf_mm) >= 0);
netbuf_delete(inbuf_mm);
}
}
netconn_close(conn_mm);
netconn_delete(conn_mm);
}
static void sp_thread(void *arg)
{
while(1)
{
udp_client_connect_sp();
sp_vfd_init();
udp_remove(upcb_sp);
}
}
static void mm_thread(void *arg)
{
while(1)
{
udp_client_connect_mm();
mm_vfd_init();
udp_remove(upcb_mm);
}
}
void sp_thread_init()
{
sys_thread_new("sp_thread", sp_thread, NULL, (configMINIMAL_STACK_SIZE*2), SP_THREAD_PRIO);
}
void mm_thread_init()
{
sys_thread_new("mm_thread", mm_thread, NULL, (configMINIMAL_STACK_SIZE*2), MM_THREAD_PRIO);
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-07-02 07:07 AM
#define SP_THREAD_PRIO ( osPriorityAboveNormal )
#define MM_THREAD_PRIO ( osPriorityNormal )