2024-12-24 08:59 PM
Hello,
Just before I tried to debug STM32L052 via ST-Link but following error occurred.
The error message is as following.
It's strange that I could debug and run with same project yesterday and nothing is changed as for project.
What is the problem and how to solve it?
Thanks,
STMicroelectronics ST-LINK GDB server. Version 7.9.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Target unknown error 19
Error in initializing ST-LINK device.
Reason: Unknown. Please check power and cabling to target.
2024-12-24 11:13 PM
Hello @curiae ,
Are you using your own customized board or ST board?
What happens if you connect in STM32CubeProgrammer ? Try to connect through STM32CubeProgrammer and set the connection mode to "Under Reset" and perform a "Full Chip Erase" to clear the flash memory.
Check the debug pins are free, reserved for Debug: How to solve debugger connection issues - STMicroelectronics Community.
If the issue is not resolved, check (through your STM32 schematic and Datasheet) the basic pins and the power supply schemes that are within their specified voltage ranges : VDD, VDDA supply, VCAP pins...