cancel
Showing results for 
Search instead for 
Did you mean: 

Convert the SDMMC FATFS firmware from HAL version 1.3.2 to HAL version 1.7.0

BBert
Associate III

I have a working example of the SDMMC FATFS demo firmware using HAL version 1.3.2. I want to convert the firmware to use HAL version 1.7.0. However, when I perform the conversion to 1.7.0 the SDMMC no longer works. Any access to the SD card results in a failure. Does anyone have any idea what the problem may be?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

They keep reengineering the driver code, watch for new callback methods, and the use of the transceiver.

Make sure you're using memory the core can access directly, for DMA on the SDMMC1 I'm pretty sure you're limited to AXI RAM

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
BBert
Associate III

@Community member​  Thanks for your reply. I have resolved this problem by porting the SDMMC app from the V170 examples. It appears to be working properly.