CMSIS DSP compilation error & Struct Initialization
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-03-09 1:15 PM
Hello,
I am trying to implementing PID in Systick Interrupt handler.I get this error after compilation in Keil MDK '' C:\Keil\ARM\CMSIS\Include\arm_math.h(268): error: &sharp5: cannot open source input file ''ARMCM4.h'': No such file or directory''. I added arm_cortexM3l_math.lib to my Project List but no Luck.I need help in this aspect.Also, I think I have a problem with Initailizing Kp, Ki & Kd '' arm_pid_instance_q15 '' struct.Please can someone tell me if my inialization is correct and if I did the right thing on CMSIS PID. ------------------------- /** * @brief Instance structure for the Q15 PID Control. */ typedef struct { q15_t A0; /**< The derived gain, A0 = Kp + Ki + Kd . */ &sharpifdef ARM_MATH_CM0 q15_t A1; q15_t A2; &sharpelse q31_t A1; /**< The derived gain A1 = -Kp - 2Kd | Kd.*/ &sharpendif q15_t state[3]; /**< The state array of length 3. */ q15_t Kp; /**< The proportional gain. */ q15_t Ki; /**< The integral gain. */ q15_t Kd; /**< The derivative gain. */ } arm_pid_instance_q15; ------------------ MY CODE WITH COMPILATION ERROR ------------------ &sharpinclude ''stm32f10x.h'' &sharpinclude ''arm_math.h'' int main(void) { uint16_t SpeedError,CorrectedSpeed; /* Variable that holds error*/ uint_16 resetStateFlag = 0; RCC->APB2ENR |= RCC_APB2ENR_AFIOEN | RCC_APB2ENR_IOPBEN; //PB0 & PB1 =>Alt Function Push Pull O/P | PB6-PB7 Alt Function Open Drain GPIOB->CRL = 0xFF4444AA; GPIOB->CRH = 0x44441111; //Configure PB8-PB11 as Output (Push Pull) GPIOB->ODR = 0x00000000; arm_pid_instance_q15 S; /* PID S Instance Structure*/ S.Kp = 2300; /* Change the member Kp of S to have the value of 2300 */ S.Ki = 150; /* Change the member Ki of S to have the value of 150 */ S.Kd = 0 /* Change the member Kd of S to have the value of 0 */ arm_pid_reset_q15(&S); /*resets the state buffer to zeros*/ arm_pid_init_q15 = {&S, resetStateFlag}; /* Initialize A0 & A1 from Kp, Ki & Kd */ if (SysTick_Config(SystemCoreClock / 1000)) { /* Capture error */ while(1); } while(1) { } } Regards Slim void SysTick_Handler(void) { CorrectedSpeed = __STATIC_INLINE q15_t arm_pid_q15(&S,SpeedError); /*PID out processed output sample*/ } #cmsis- Labels:
-
CMSIS
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-03-09 1:27 PM
The error is not about adding library files, you need to set up the ''Include Paths'' for the project to point at the assorted directories you have include files stored in related to the project. If the inclusion isn't required you might also want to consider if you have the right defines for the project too.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-09-29 2:20 PM
Dear Sir:
Please give me help.I use IAR 6,60.1.5104 and try to run arm_fft_bin_example_f32.c I copy arm_fft_bin_example_f32.c and arm_fft_bin_data.c under C:\...\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0\Project\testfft\and copy EWARM to same directory and add C compiler->Preprocess-> Additional include directories as$PROJ_DIR$\..\$PROJ_DIR$\..\..\..\Libraries\STM32F4xx_StdPeriph_Driver\inc$PROJ_DIR$\..\..\..\Utilities\STM32_EVAL\Common$PROJ_DIR$\..\..\..\Libraries\CMSIS\Device\ST\STM32F4xx\Include$PROJ_DIR$\..\..\..\Libraries\CMSIS\Include''Defined symbols'' asUSE_STDPERIPH_DRIVERSTM32F427XUSE_STM324x7I_EVALWhen I ''rebuild all'' it give me an error as followingarm_fft_bin_data.c Fatal Error[Pe1696]: cannot open source file ''ARMCM4.h'' C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Libraries\CMSIS\Include\arm_math.h 269 searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Libraries\CMSIS\Include\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\EWARM\..\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\EWARM\..\..\..\Libraries\STM32F4xx_StdPeriph_Driver\inc\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\EWARM\..\..\..\Utilities\STM32_EVAL\Common\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\EWARM\..\..\..\Libraries\CMSIS\Device\ST\STM32F4xx\Include\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\EWARM\..\..\..\Libraries\CMSIS\Include\'' searched: ''C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\'' searched: ''C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\inc\'' searched: ''C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\inc\c\'' Error while running C/C++ Compiler arm_fft_bin_example_f32.c Fatal Error[Pe1696]: cannot open source file ''ARMCM4.h'' C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Libraries\CMSIS\Include\arm_math.h 269 searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Libraries\CMSIS\Include\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\EWARM\..\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\EWARM\..\..\..\Libraries\STM32F4xx_StdPeriph_Driver\inc\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\EWARM\..\..\..\Utilities\STM32_EVAL\Common\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\EWARM\..\..\..\Libraries\CMSIS\Device\ST\STM32F4xx\Include\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\EWARM\..\..\..\Libraries\CMSIS\Include\'' searched: ''C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\'' searched: ''C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\inc\'' searched: ''C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\inc\c\'' Error while running C/C++ Compiler Thank you very much.Yu Tang- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-09-29 4:55 PM
You need the define ARM_MATH_CM4, otherwise is falls through and looks for an include you clearly don't have.
From the instructions in STM32F4xx_DSP_StdPeriph_Lib_V1.2.0\Libraries\CMSIS\Include\arm_math.h* The library functions are declared in the public file <
code
>arm_math.h</
code
> which is placed in the <
code
>Include</
code
> folder.
* Simply include this file and link the appropriate library in the application and begin calling the library functions. The Library supports single
* public header file <
code
> arm_math.h</
code
> for Cortex-M4/M3/M0 with little endian and big endian. Same header file will be used for floating point unit(FPU) variants.
* Define the appropriate pre processor MACRO ARM_MATH_CM4 or ARM_MATH_CM3 or
* ARM_MATH_CM0 or ARM_MATH_CM0PLUS depending on the target processor in the application.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-09-30 10:35 AM
Dear Sir:
Yes, I put #define
ARM_MATH_CM4 at beginning of arm_fft_bin_example_f32.c, but it give me error as following, please help to figure out the problem.
Fatal Error[Pe1696]: cannot open source file ''ARMCM4.h'' C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 280 searched: ''C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\EWARM\..\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\EWARM\..\..\..\Libraries\CMSIS\Device\ST\STM32F4xx\Include\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\EWARM\..\..\..\Libraries\STM32F4xx_StdPeriph_Driver\inc\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\EWARM\..\..\..\Utilities\STM32_EVAL\Common\'' searched: ''C:\aKopin\0VC\STM32F4xx_DSP_StdPeriph_Lib_V1.1.0y\Project\testfft\EWARM\..\..\..\Utilities\STM32_EVAL\STM3240_41_G_EVAL\'' searched: ''C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\inc\'' searched: ''C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\inc\c\'' Error while running C/C++ Compiler arm_fft_bin_example_f32.c Error[Pe011]: unrecognized preprocessing directive C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\core_cm4.h 124 Warning[Pe011]: unrecognized preprocessing directive C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 281 Warning[Pa031]: IAR keyword ''__packed'' used with IAR extended language disabled C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4971 Error[Pe065]: expected a '';'' C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4971 Error[Pe020]: identifier ''vstate'' is undefined C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4979 Error[Pe018]: expected a '')'' C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4979 Warning[Pe177]: variable ''__packed'' was declared but never referenced C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4971 Error while running C/C++ CompilerThank you very much.
Yu Tang- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-09-30 11:20 AM
define
ARM_MATH_CM4 at beginning of arm_fft_bin_example_f32.c, but it give me error as following, please help to figure out the problem.
Changing the source code of the library is a rather bad idea. Define ARM_MATH_CM4 on projects settings level, for instance in CPPFLAGS in the Makefile (or whatever your project is based on). You might need to come to grips with you toolchain, the C language, and your build environment.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-09-30 11:58 AM
Not much into IAR, but you'll want the define globally, along with the USE_STDPERIPH_DRIVER, etc for the pre-processor.
The define clearly isn't being set, based on the include it's trying to pull in.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-09-30 12:56 PM
I put it, now the Defined Symbol as
USE_STDPERIPH_DRIVERSTM32F40XXUSE_STM324xG_EVALARM_MATH_CM4but I get new errors as followingarm_fft_bin_data.c Error[Pe011]: unrecognized preprocessing directive C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\core_cm4.h 124 Warning[Pe011]: unrecognized preprocessing directive C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 281 Warning[Pa031]: IAR keyword ''__packed'' used with IAR extended language disabled C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4971 Error[Pe065]: expected a '';'' C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4971 Error[Pe020]: identifier ''vstate'' is undefined C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4979 Error[Pe018]: expected a '')'' C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4979 Warning[Pe177]: variable ''__packed'' was declared but never referenced C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4971 Error while running C/C++ Compiler arm_fft_bin_example_f32.c Error[Pe011]: unrecognized preprocessing directive C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\core_cm4.h 124 Warning[Pe011]: unrecognized preprocessing directive C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 281 Warning[Pa031]: IAR keyword ''__packed'' used with IAR extended language disabled C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4971 Error[Pe065]: expected a '';'' C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4971 Error[Pe020]: identifier ''vstate'' is undefined C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4979 Error[Pe018]: expected a '')'' C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4979 Warning[Pe177]: variable ''__packed'' was declared but never referenced C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4971 Error while running C/C++ Compiler Please give me another help, thank you very much.Yu- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-09-30 12:57 PM
I put it, now the Defined Symbol as
USE_STDPERIPH_DRIVERSTM32F40XXUSE_STM324xG_EVALARM_MATH_CM4but I get new errors as followingarm_fft_bin_data.c Error[Pe011]: unrecognized preprocessing directive C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\core_cm4.h 124 Warning[Pe011]: unrecognized preprocessing directive C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 281 Warning[Pa031]: IAR keyword ''__packed'' used with IAR extended language disabled C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4971 Error[Pe065]: expected a '';'' C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4971 Error[Pe020]: identifier ''vstate'' is undefined C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4979 Error[Pe018]: expected a '')'' C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4979 Warning[Pe177]: variable ''__packed'' was declared but never referenced C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4971 Error while running C/C++ Compiler arm_fft_bin_example_f32.c Error[Pe011]: unrecognized preprocessing directive C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\core_cm4.h 124 Warning[Pe011]: unrecognized preprocessing directive C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 281 Warning[Pa031]: IAR keyword ''__packed'' used with IAR extended language disabled C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4971 Error[Pe065]: expected a '';'' C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4971 Error[Pe020]: identifier ''vstate'' is undefined C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4979 Error[Pe018]: expected a '')'' C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4979 Warning[Pe177]: variable ''__packed'' was declared but never referenced C:\Program Files (x86)\IAR Systems\Embedded Workbench 6.5\arm\CMSIS\Include\arm_math.h 4971 Error while running C/C++ CompilerPlease give me another help, thank you very much.
Yu- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-09-30 2:35 PM
Now it seems to be pulling include files from within IAR rather than those pathed within the DSP library. Secondarily it is complaining about ''packed'' and needing extended language features enabled. As you're using IAR, you should probably seek support from them after you have reviewed the manuals/documentation for your tool chain.
Are there any pre built project examples within the DSP library?Up vote any posts that you find helpful, it shows what's working..