cancel
Showing results for 
Search instead for 
Did you mean: 

Checking (HAL_TIMEx_MasterConfigSynchronization(&htim12, &sMasterConfig) != HAL_OK), halt the system

Abid
Associate II

I am using STM32F407 with eclipse IDE. And I want to generate PWM signal using TIMER12. After all the configuration, when I call,

 

"sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim12, &sMasterConfig) != HAL_OK) { Error_Handler(); }"

 

 

inside MX_TIM12_Init(); function, the MCU just stuck and I get no print function.

On debugger console I get a the following message,

"Wrong parameters value: file ../../stm32f4-hal/stm32f4xx_hal_tim_ex.c on line 1636".

And this line refers to the following lines of codes,

 

 

" HAL_StatusTypeDef HAL_TIMEx_MasterConfigSynchronization(TIM_HandleTypeDef *htim, TIM_MasterConfigTypeDef *sMasterConfig) { uint32_t tmpcr2; uint32_t tmpsmcr; /* Check the parameters */ assert_param(IS_TIM_MASTER_INSTANCE(htim->Instance)); assert_param(IS_TIM_TRGO_SOURCE(sMasterConfig->MasterOutputTrigger)); assert_param(IS_TIM_MSM_STATE(sMasterConfig->MasterSlaveMode)); /* Check input state */ __HAL_LOCK(htim); /* Change the handler state */ htim->State = HAL_TIM_STATE_BUSY; /* Get the TIMx CR2 register value */ tmpcr2 = htim->Instance->CR2; /* Get the TIMx SMCR register value */ tmpsmcr = htim->Instance->SMCR; /* Reset the MMS Bits */ tmpcr2 &= ~TIM_CR2_MMS; /* Select the TRGO source */ tmpcr2 |= sMasterConfig->MasterOutputTrigger; /* Update TIMx CR2 */ htim->Instance->CR2 = tmpcr2; if (IS_TIM_SLAVE_INSTANCE(htim->Instance)) { /* Reset the MSM Bit */ tmpsmcr &= ~TIM_SMCR_MSM; /* Set master mode */ tmpsmcr |= sMasterConfig->MasterSlaveMode; /* Update TIMx SMCR */ htim->Instance->SMCR = tmpsmcr; } /* Change the htim state */ htim->State = HAL_TIM_STATE_READY; __HAL_UNLOCK(htim); return HAL_OK; }".
View more

 

What could be possible reason?

1 ACCEPTED SOLUTION

Accepted Solutions
Abid
Associate II

@TDK wrote:

Yep, this is exactly it. TIM12 was not a master timer on very old HAL versions. It is fixed in the latest version.

https://github.com/STMicroelectronics/STM32CubeF4/blob/55c4943bb82fce7bd64577949eebcabd20e9cf1b/Drivers/CMSIS/Device/ST/STM32F4xx/Include/stm32f407xx.h#L15280

 


I am not using the old version. 

And I think, I found the problem. Problem was in following statement. 

 

#ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @PAram file: pointer to the source file name * @PAram line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */

 

 In eclipse IDE it is defined in the STM32_assert.h file. I move it in main.c file and the problem is gone. 

View solution in original post

3 REPLIES 3
TDK
Super User

Probably the parameter on line 1636 is invalid. You can check the IS_TIM_* macros to be sure.

Seems like your HAL library version is quite a bit out of date as the current library has that function starting on line 1964. It could be due to a bug that has been fixed.

https://github.com/STMicroelectronics/STM32CubeF4/blob/master/Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_tim_ex.c#L1964

 

If you feel a post has answered your question, please click "Accept as Solution".
TDK
Super User

Yep, this is exactly it. TIM12 was not a master timer on very old HAL versions. It is fixed in the latest version.

https://github.com/STMicroelectronics/STM32CubeF4/blob/55c4943bb82fce7bd64577949eebcabd20e9cf1b/Drivers/CMSIS/Device/ST/STM32F4xx/Include/stm32f407xx.h#L15280

 

If you feel a post has answered your question, please click "Accept as Solution".
Abid
Associate II

@TDK wrote:

Yep, this is exactly it. TIM12 was not a master timer on very old HAL versions. It is fixed in the latest version.

https://github.com/STMicroelectronics/STM32CubeF4/blob/55c4943bb82fce7bd64577949eebcabd20e9cf1b/Drivers/CMSIS/Device/ST/STM32F4xx/Include/stm32f407xx.h#L15280

 


I am not using the old version. 

And I think, I found the problem. Problem was in following statement. 

 

#ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @PAram file: pointer to the source file name * @PAram line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */

 

 In eclipse IDE it is defined in the STM32_assert.h file. I move it in main.c file and the problem is gone.