cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot Extract STSW-SAFEA1-MW

rlederhose
Associate

Hi,

I am having trouble extracting the STSW-SAFEA1-MW. This is the same issue mentioned here and here. I can't use your product if I can't use your drivers. A fix would be appreciated.

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @rlederhose, to the community!

I also tested this again after @Frantz LEFRERE tried it here and also had problems with some unzip programmes. However, the ZIP can be unpacked very well with the open source (un)packer 7-z.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome @rlederhose, to the community!

I also tested this again after @Frantz LEFRERE tried it here and also had problems with some unzip programmes. However, the ZIP can be unpacked very well with the open source (un)packer 7-z.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks for the help Peter! 7zip worked a treat.