2025-01-08 07:21 PM
Hi,
I am having trouble extracting the STSW-SAFEA1-MW. This is the same issue mentioned here and here. I can't use your product if I can't use your drivers. A fix would be appreciated.
Thanks
Solved! Go to Solution.
2025-01-08 11:33 PM
Welcome @rlederhose, to the community!
I also tested this again after @Frantz LEFRERE tried it here and also had problems with some unzip programmes. However, the ZIP can be unpacked very well with the open source (un)packer 7-z.
Hope that helps?
Regards
/Peter
2025-01-08 11:33 PM
Welcome @rlederhose, to the community!
I also tested this again after @Frantz LEFRERE tried it here and also had problems with some unzip programmes. However, the ZIP can be unpacked very well with the open source (un)packer 7-z.
Hope that helps?
Regards
/Peter
2025-01-09 03:05 AM
Thanks for the help Peter! 7zip worked a treat.