cancel
Showing results for 
Search instead for 
Did you mean: 

Can the USBPD software be used without the TCPP hardware?

Carl_G
Associate II

I need to have USB PD connectivity so I am using the examples provided. There are SNK and SRC and DRP examples. However, they all use the TCPP which is also included in all of the 3 demo boards. I don't see any way to disable the TCPP component itself and keep using the X-CUBE-TCPP middleware because it seems there is a library file provided that has the TCPP manipulation within it and I can't edit that file.

Is there any recommended strategy for developing a USBPD application on the STM32G071 that does not include the use of the TCPP hardware? I can uncheck the Board Part and the Board Support package but then I don't get good code generation.

 

Thanks

0 REPLIES 0