Bug report STM32CubeMX 4.25.0 - Activating ''Audio Clock Input'' (I2S_CKIN) does not set I2SSRC bit in RCC_CFGR register
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-03-29 11:08 PM
I have a project generated by &sharpSTM32CubeMX 4.25.0 using firmware STM32Cube FW_F4 V1.21.0. The clock configuration can be found in the attached picture below. When I debugged the generated code I have seen that I2SSRC bit in RCC_CFGR register was not set to 1; which causes I2S malfunctioning. Here is the code generated by CubeMX:I have a project generated by &sharpSTM32CubeMX 4.25.0 using firmware STM32Cube FW_F4 V1.21.0. The clock configuration can be found in the attached picture below. When I debugged the generated code I have seen that I2SSRC bit in RCC_CFGR register was not set to 1; which causes I2S malfunctioning. Here is the code generated by CubeMX:I have a project generated by &sharpSTM32CubeMX 4.25.0 using firmware STM32Cube FW_F4 V1.21.0. The clock configuration can be found in the attached picture below. When I debugged the generated code I have seen that I2SSRC bit in RCC_CFGR register was not set to 1; which causes I2S malfunctioning. Here is the code generated by CubeMX:I have a project generated by &sharpSTM32CubeMX 4.25.0 using firmware STM32Cube FW_F4 V1.21.0. The clock configuration can be found in the attached picture below. When I debugged the generated code I have seen that I2SSRC bit in RCC_CFGR register was not set to 1; which causes I2S malfunctioning. Here is the code generated by CubeMX:
/* I2S3 init function */
void MX_I2S3_Init(void){hi2s3.Instance = SPI3;
hi2s3.Init.Mode = I2S_MODE_MASTER_TX; hi2s3.Init.Standard = I2S_STANDARD_PHILIPS; hi2s3.Init.DataFormat = I2S_DATAFORMAT_16B; hi2s3.Init.MCLKOutput = I2S_MCLKOUTPUT_DISABLE; hi2s3.Init.AudioFreq = I2S_AUDIOFREQ_8K; hi2s3.Init.CPOL = I2S_CPOL_LOW; hi2s3.Init.ClockSource = I2S_CLOCK_EXTERNAL; hi2s3.Init.FullDuplexMode = I2S_FULLDUPLEXMODE_ENABLE; if (HAL_I2S_Init(&hi2s3) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
void HAL_I2S_MspInit(I2S_HandleTypeDef* i2sHandle)
{GPIO_InitTypeDef GPIO_InitStruct;
if(i2sHandle->Instance==SPI3) { /* USER CODE BEGIN SPI3_MspInit 0 *//* USER CODE END SPI3_MspInit 0 */
/* I2S3 clock enable */ __HAL_RCC_SPI3_CLK_ENABLE(); /**I2S3 GPIO Configuration PA4 ------> I2S3_WS PC10 ------> I2S3_CK PC11 ------> I2S3_ext_SD PC12 ------> I2S3_SD */ GPIO_InitStruct.Pin = GPIO_PIN_4; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM; GPIO_InitStruct.Alternate = GPIO_AF6_SPI3; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);GPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM; GPIO_InitStruct.Alternate = GPIO_AF6_SPI3; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);GPIO_InitStruct.Pin = GPIO_PIN_11;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM; GPIO_InitStruct.Alternate = GPIO_AF5_I2S3ext; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);/* I2S3 DMA Init */
/* I2S3_EXT_RX Init */ hdma_i2s3_ext_rx.Instance = DMA1_Stream0; hdma_i2s3_ext_rx.Init.Channel = DMA_CHANNEL_3; hdma_i2s3_ext_rx.Init.Direction = DMA_PERIPH_TO_MEMORY; hdma_i2s3_ext_rx.Init.PeriphInc = DMA_PINC_DISABLE; hdma_i2s3_ext_rx.Init.MemInc = DMA_MINC_ENABLE; hdma_i2s3_ext_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD; hdma_i2s3_ext_rx.Init.MemDataAlignment = DMA_MDATAALIGN_WORD; hdma_i2s3_ext_rx.Init.Mode = DMA_CIRCULAR; hdma_i2s3_ext_rx.Init.Priority = DMA_PRIORITY_HIGH; hdma_i2s3_ext_rx.Init.FIFOMode = DMA_FIFOMODE_ENABLE; hdma_i2s3_ext_rx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL; hdma_i2s3_ext_rx.Init.MemBurst = DMA_MBURST_SINGLE; hdma_i2s3_ext_rx.Init.PeriphBurst = DMA_PBURST_SINGLE; if (HAL_DMA_Init(&hdma_i2s3_ext_rx) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }__HAL_LINKDMA(i2sHandle,hdmarx,hdma_i2s3_ext_rx);
/* SPI3_TX Init */
hdma_spi3_tx.Instance = DMA1_Stream5; hdma_spi3_tx.Init.Channel = DMA_CHANNEL_0; hdma_spi3_tx.Init.Direction = DMA_MEMORY_TO_PERIPH; hdma_spi3_tx.Init.PeriphInc = DMA_PINC_DISABLE; hdma_spi3_tx.Init.MemInc = DMA_MINC_ENABLE; hdma_spi3_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD; hdma_spi3_tx.Init.MemDataAlignment = DMA_MDATAALIGN_WORD; hdma_spi3_tx.Init.Mode = DMA_CIRCULAR; hdma_spi3_tx.Init.Priority = DMA_PRIORITY_HIGH; hdma_spi3_tx.Init.FIFOMode = DMA_FIFOMODE_ENABLE; hdma_spi3_tx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL; hdma_spi3_tx.Init.MemBurst = DMA_MBURST_SINGLE; hdma_spi3_tx.Init.PeriphBurst = DMA_PBURST_SINGLE; if (HAL_DMA_Init(&hdma_spi3_tx) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }__HAL_LINKDMA(i2sHandle,hdmatx,hdma_spi3_tx);
/* USER CODE BEGIN SPI3_MspInit 1 */
/* USER CODE END SPI3_MspInit 1 */
}}#stm32cubemx-4.25.0 #i2ssrc #stm32f4 #rcc_cfgr #audio-clock-input- Labels:
-
Audio
-
I2S
-
RCC
-
STM32CubeMX
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-04-03 08:12 AM
Hi
metecantimur
,Could you please precise on which device you have found the issue. So, we can verify it.
Best Regards,
Imen
Thanks
Imen
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-04-04 01:32 AM
Hi
DAHMEN.IMEN
,I am using STM32F407ZGTx MCU device in an proprietary board.
Best Regards,
Mete
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-04-04 07:44 AM
Hi
DAHMEN.IMEN
,I have the following workaround steps for the problem:
1) Insert the following line into the function
HAL_I2S_MspInitjust before the line containing __HAL_RCC_SPI3_CLK_ENABLE();
/* BUG FIX: Enabling Audio Clock Input in CubeMX does not set I2SSRC bit
* in RCC_CFGR register! Hence we need to set it manually here! * WARNING: A bug fix is also needed in __HAL_RCC_GET_I2S_SOURCE() */
__HAL_RCC_I2S_CONFIG(RCC_I2SCLKSOURCE_EXT);
2) Apply the following patch to the following macro in library the file 'stm32f4xx_hal_rcc_ex.h' at line 6112:
#define __HAL_RCC_GET_I2S_SOURCE() ((uint32_t)(READ_BIT(RCC->CFGR, RCC_CFGR_I2SSRC)) >> RCC_CFGR_I2SSRC_Pos) /*BUG FIX: MC*/
Note: I will report the bug in filestm32f4xx_hal_rcc_ex.h
at line 6112 as a new bug report.
Best Regards,
Mete