cancel
Showing results for 
Search instead for 
Did you mean: 

Bug in LL library for stm32f1xx

amomum
Associate III
Posted on September 27, 2017 at 19:03

I want to turn on the led attached to PC.9. I do this:

    LL_GPIO_InitTypeDef initStruct;

    LL_GPIO_StructInit( &initStruct );

    

    initStruct.Mode = LL_GPIO_MODE_OUTPUT_10MHz;

    initStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;

    initStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;

    initStruct.Pin = LL_GPIO_PIN_9; // that equals 0x04020002

    

    LL_GPIO_Init( GPIOC, &initStruct )

This code will actually init PC.2 (not PC.9 as it's supposed to) to output push-pull.

Why? LL_GPIO_Init does this:

    pinpos = POSITION_VAL(GPIO_InitStruct->Pin);

where

    &sharpdefine POSITION_VAL(VAL)     (__CLZ(__RBIT(VAL)))

so pinpos will be equal to 

(__CLZ(__RBIT(

0x04020002

))) which is equal to 1.

Then current pin will be calculated like this:

    currentpin = (GPIO_InitStruct->Pin) & (0x00000101U << pinpos);

so currentpint will be equal to 2.

And then

    LL_GPIO_SetPinMode(GPIOx, currentpin, GPIO_InitStruct->Mode);

will be called, despite the fact that LL_GPIO_SetPinMode should only accept parameters like LL_GPIO_PIN_x.

Reasons:

  •   all inline functions in header files do not check their arguments with assert_param, so this error was not caught early
  •   lack of proper (i.e. automatic) testing?
  •   lack of public bugtracker

I have already posted this bug here but it got mixed up with my own ignorance and stupidity so I haven't got a proper reaction. I believe it's time to post it again.

#hal-ll #ll-bug #software-error #bug #ll #stm32f1
This discussion is locked. Please start a new topic to ask your question.
20 REPLIES 20
Posted on February 19, 2018 at 09:44

If we decide to fix the issue. I well share it.

But first we have to figure out what the best solution would be for us. It seems that the LL for the STM32F1xx devices is a unstable release if a fundamental function like the pin initialization is not working.  

Best regards Raphael

Posted on February 19, 2018 at 11:05

Simon Brouwer already posted a fix of the issue in his first response. Thanks for the work and sorry for overriding the post. 

Best regards Raphael

Posted on February 19, 2018 at 11:32

Thank you for letting me know. I just missed it. Probably because I did quick hack for myself.

Posted on February 19, 2018 at 12:01

Hello,

This issue is confirmed for LL Gpio pins greater than 8 initialization with LL-Init() function and this will be fixed in the next release.

We propose thisfix for LL_GPIO_Init function in the ll_gpio.c driver:

ErrorStatus LL_GPIO_Init(GPIO_TypeDef *GPIOx, LL_GPIO_InitTypeDef *GPIO_InitStruct)
{
 uint32_t pinmask = 0x00000000U;
 uint32_t pinpos = 0x00000000U;
 uint32_t currentpin = 0x00000000U;
 
 /* Check the parameters */
 assert_param(IS_GPIO_ALL_INSTANCE(GPIOx));
 assert_param(IS_LL_GPIO_PIN(GPIO_InitStruct->Pin));
 assert_param(IS_LL_GPIO_MODE(GPIO_InitStruct->Mode));
 assert_param(IS_LL_GPIO_PULL(GPIO_InitStruct->Pull));
 
 /* ------------------------- Configure the port pins ---------------- */
 /* Initialize pinpos on first pin set */
 
 pinmask = (GPIO_InitStruct->Pin & 0x00FFFF00U) >> 8 ;
 pinpos = POSITION_VAL(pinmask);
/* Configure the port pins */
 while ((pinmask >> pinpos) != 0U)
 {
 /* skip if bit is not set */
 if ((pinmask & (1U << pinpos)) == 0U)
 {
 pinpos++;
 }
/* Get current io position */
 if(pinpos <8 )
 {
 currentpin = (0x00000101U << pinpos);
 }
 else
 {
 currentpin = ((0x00010001U << (pinpos-8)) | 0x04000000U);
 }
 
 if (currentpin)
 {
 /* Pin Mode configuration */
 LL_GPIO_SetPinMode(GPIOx, currentpin, GPIO_InitStruct->Mode);
 
 /* Pull-up Pull down resistor configuration*/
 LL_GPIO_SetPinPull(GPIOx, currentpin, GPIO_InitStruct->Pull);
 
 if ((GPIO_InitStruct->Mode == LL_GPIO_MODE_OUTPUT) || (GPIO_InitStruct->Mode == LL_GPIO_MODE_ALTERNATE))
 {
 /* Check Output mode parameters */
 assert_param(IS_LL_GPIO_OUTPUT_TYPE(GPIO_InitStruct->OutputType));
/* Output mode configuration*/
 LL_GPIO_SetPinOutputType(GPIOx, currentpin, GPIO_InitStruct->OutputType);
/* Speed mode configuration */
 LL_GPIO_SetPinSpeed(GPIOx, currentpin, GPIO_InitStruct->Speed);
 }
}
 pinpos++;
 }
 return (SUCCESS);
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

Hope this is helpful for you.

Kind Regards,

Imen.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on February 19, 2018 at 21:38

Hi Imen, I think if you leave out the 'continue; ', some pins may be affected that correspond to a 0 bit in the pinmask (after skipping the first 0 bit, the next pin will be configured even if its bit in the pinmask is 0)

Posted on March 09, 2018 at 15:23

Hi Imen,

ST should pay more attention when proposing code as a workaround.

If one wants to gloss over the pre-existing overcomplicated and bizarre definition of the pin constants for the F1, justified only by a small possible saving in scarcely used initialization routines, the proposed code is both redundant, as

  • it pointlessly initialize variables that will always be set
  • it checks currrentpin for inequality to 0, guaranteed by the statement right above the check

and wrong, as Simon Brouwer already pointed out.

Is there a publicly accessible bug tracker for the LL_ library (and the HAL)?

Posted on March 12, 2018 at 11:02

Hello

simon.010

,

Your proposal fix is raised internally to developer team for check.

Thanks andBest Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on March 16, 2018 at 19:20

Just tested a STM32VLDIscovery board and the issue still exists in CubeMX 4.25.0 with the v1.6.0 HAL/LL drivers.

Posted on March 19, 2018 at 17:08

Just tested STM32CubeF1 Firmware patch Package V1.6.1 - GPIO works fine.

Imen.D
ST Employee
Posted on March 22, 2018 at 09:53

Hello,

We would inform you that the new patch of STM32CubeF1 Firmware package V1.6.1 is released to fix this issue.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen