cancel
Showing results for 
Search instead for 
Did you mean: 

Bug in LL library for stm32f1xx

amomum
Associate III
Posted on September 27, 2017 at 19:03

I want to turn on the led attached to PC.9. I do this:

    LL_GPIO_InitTypeDef initStruct;

    LL_GPIO_StructInit( &initStruct );

    

    initStruct.Mode = LL_GPIO_MODE_OUTPUT_10MHz;

    initStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;

    initStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;

    initStruct.Pin = LL_GPIO_PIN_9; // that equals 0x04020002

    

    LL_GPIO_Init( GPIOC, &initStruct )

This code will actually init PC.2 (not PC.9 as it's supposed to) to output push-pull.

Why? LL_GPIO_Init does this:

    pinpos = POSITION_VAL(GPIO_InitStruct->Pin);

where

    &sharpdefine POSITION_VAL(VAL)     (__CLZ(__RBIT(VAL)))

so pinpos will be equal to 

(__CLZ(__RBIT(

0x04020002

))) which is equal to 1.

Then current pin will be calculated like this:

    currentpin = (GPIO_InitStruct->Pin) & (0x00000101U << pinpos);

so currentpint will be equal to 2.

And then

    LL_GPIO_SetPinMode(GPIOx, currentpin, GPIO_InitStruct->Mode);

will be called, despite the fact that LL_GPIO_SetPinMode should only accept parameters like LL_GPIO_PIN_x.

Reasons:

  •   all inline functions in header files do not check their arguments with assert_param, so this error was not caught early
  •   lack of proper (i.e. automatic) testing?
  •   lack of public bugtracker

I have already posted this bug here but it got mixed up with my own ignorance and stupidity so I haven't got a proper reaction. I believe it's time to post it again.

#hal-ll #ll-bug #software-error #bug #ll #stm32f1
This discussion is locked. Please start a new topic to ask your question.
20 REPLIES 20
amomum
Associate III
Posted on March 27, 2018 at 12:51

I'm glad that this issue is finally fixed but I'm startled that we still have to use community forum to submit issues about code. Moderators have to manually search for bugs and repost them in bug-tracker, users have to wait for several months just to be noticed!

Please, ST, please, make bug-tracker for code public! Or - better - make repository public (all of the code is open-source anyway, so why hide it?), a lot of the users will be glad to help with code.