2024-03-20 01:50 AM
Hey. Is it possible to execute code from external memory using only single- or dual-SPI mode? I have a PCB here with a STM32H730 CPU, but on the flash memory, WP/SIO2 and RESET/SIO3 are connected, so no Quad-SPI possible.
In these official references concerning XiP I only find Quad-SPI or Dual-Quad(=Octo)-SPI mentioned:
- AN5188
- AN4760 section 6.2
- https://www.youtube.com/watch?v=YFIvJVsvIsE&list=PLnMKNibPkDnHIrq5BICcFhLsmJFI_ytvE&index=2
Thank You!
Solved! Go to Solution.
2024-03-20 02:51 AM
Yes
If you can construct a read command and access the memory, you can use that as a template for the Memory Mapped mode.
Single or Dual will work fine, although will constrain bandwidth. Caching properly can hide a lot of that.
2024-03-20 02:51 AM
Yes
If you can construct a read command and access the memory, you can use that as a template for the Memory Mapped mode.
Single or Dual will work fine, although will constrain bandwidth. Caching properly can hide a lot of that.
2024-03-20 06:06 AM - edited 2024-03-20 06:12 AM
Ah, thank You very much, good news. So, I'll try this.
To get it right: By "use that as a template" You mean setting the right commands for instance into OCTOSPI_IR and OCTOSPI_WIR registers? Ist this special in Single- or Dual-SPI-Usage of Memory-mapped mode, or wouldn't I have to put the commands there anyway, also in Quad-SPI (unless my HAL or any other layer doesn't put some proper / common / default commands there)?