2023-11-27 11:58 PM
Hi, I have a circuit in which I want to check every cycle if a measured voltage is over a limit value and in that case disable the measure over one of four DUTs forcing to LOW the state of some pins. The problem is that in the main loop I have command line that set the state of the pin sometimes to high and sometimes to low and I would to find a way to block the state of a pin and do not change his state until the end of the program. I thought to use the IF but I have 4 DUTs to check and control separately.
2023-11-28 12:41 AM
You haven't told us which STM32 and which pins, so just a vague answer:
One of the tricks could be setting the pin to AF to a peripheral which can hold it low, e.g. timer. After that, writes to GPIOx_ODR (directly or through GPIOx_BSRR) won't be reflected on the pin's state.
Nonetheless, this is not something you can click in CubeMX.
JW
2023-11-28 6:39 AM
Can't you implement this in program logic?
If out of bounds, don't change pin state.
I don't see how having 4 pins like this changes anything. If you have an array for them, you can do the check there. If not, four separate statements will work.