Skip to main content
CWern.1
Associate II
June 9, 2021
Question

Behavior with _LOW_POWER

Hi everyone,

I am working on an USB-PD source that is battery powered.

To make use of the low power features, I defined _LOW_POWER.

When this is defined, I get a problem in connection with eletronically marked cables (EMC). Non-EMC cables work fine.

The system will get stuck in the state currentHWcondition "HW_PwrCable_NoSink_Attachment".

I investigated the issue and found that the system works perfectly once I commented the following lines in usbpd_cad_hw_if.c related to _LOW_POWER

uint32_t CAD_StateMachine(uint8_t PortNum, USBPD_CAD_EVENT *pEvent, CCxPin_TypeDef *pCCXX)
{
 CAD_HW_HandleTypeDef *_handle = &CAD_HW_Handles[PortNum];
 uint32_t _timing = CAD_DEFAULT_TIME;
 
 /* set by default event to none */
 *pEvent = USBPD_CAD_EVENT_NONE;
 
 if (USBPD_TRUE == Ports[PortNum].params->PE_SwapOngoing)
 {
 return _timing;
 }
 
 if (_handle->CAD_ErrorRecoveryflag == USBPD_TRUE)
 {
 /* Force the state error recovery */
 _handle->CAD_ErrorRecoveryflag = USBPD_FALSE;
 _handle->cstate = USBPD_CAD_STATE_ERRORRECOVERY;
#if defined(_TRACE)
 USBPD_TRACE_Add(USBPD_TRACE_CAD_LOW, PortNum, (uint8_t)_handle->cstate, NULL, 0);
#endif /* _TRACE */
 }
 
 switch(_handle->cstate)
 {
 case USBPD_CAD_STATE_RESET:
 {
//#if !defined(_LOW_POWER) && !defined(USBPDM1_VCC_FEATURE_ENABLED)
		//DBG
 LL_UCPD_EnableIT_TypeCEventCC2(Ports[PortNum].husbpd);
 LL_UCPD_EnableIT_TypeCEventCC1(Ports[PortNum].husbpd);
//#endif /* !_LOW_POWER */
 if( 0 == PortNum)
 {
 UCPD_INSTANCE0_ENABLEIRQ;
 }
#if USBPD_PORT_COUNT > 1
 else
 {
 UCPD_INSTANCE1_ENABLEIRQ;
 }
#endif /* USBPD_PORT_COUNT > 1 */
#if defined(_DRP) || defined(_ACCESSORY_SNK)
 _handle->CAD_tToggle_start = HAL_GetTick();
#endif /* _DRP || _ACCESSORY_SNK */
 _handle->cstate = USBPD_CAD_STATE_DETACHED;
 break;
 }
void CAD_Check_HW_SRC(uint8_t PortNum)
{
#if !defined(_RTOS)
 uint32_t CC1_value_temp, CC2_value_temp;
#endif /* !_RTOS */
 CAD_HW_HandleTypeDef *_handle = &CAD_HW_Handles[PortNum];
 /* done to prevent code optimization issue with GCC */
 uint32_t CC1_value, CC2_value;
 
 /*
 ----------------------------------------------------------------------------
 | ANAMODE | ANASUBMODE[1:0] | Notes | TYPEC_VSTATE_CCx[1:0] |
 | | | | 00 | 01 | 10 | 11 |
 ----------------------------------------------------------------------------
 | 0: Source | 00: Disabled |Disabled N/A | NA |
 | | 01: Default USB Rp| |vRaDef|vRdDef|vOPENDef| |
 | | 10: 1.5A Rp | |vRa1.5|vRd1.5|vOPEN1.5| NA |
 | | 11: 3.0A Rp | |vRa3.0|vRd3.0|vOPEN3.0| NA |
 -----------------------------------------------------------------------------
 | 1: Sink | | |xx vRa|vRdUSB| vRd1.5 |vRd3.0|
 -----------------------------------------------------------------------------
 */
//DBG
//#ifdef _LOW_POWER
// /* Enable type C state machine */
// CLEAR_BIT(Ports[PortNum].husbpd->CR, UCPD_CR_CC1TCDIS | UCPD_CR_CC2TCDIS);
 
// for(int32_t index=0; index < 200/2; index++){ __DSB();};
//#endif /* _LOW_POWER */
 
 CC1_value = (Ports[PortNum].husbpd->SR & UCPD_SR_TYPEC_VSTATE_CC1) >> UCPD_SR_TYPEC_VSTATE_CC1_Pos;
 CC2_value = (Ports[PortNum].husbpd->SR & UCPD_SR_TYPEC_VSTATE_CC2) >> UCPD_SR_TYPEC_VSTATE_CC2_Pos;
//DBG
//#ifdef _LOW_POWER
// /* Disable the C state machine */
// SET_BIT(Ports[PortNum].husbpd->CR, UCPD_CR_CC1TCDIS | UCPD_CR_CC2TCDIS);
//#endif /* _LOW_POWER */
 

Is this a known issue or am I using the code wrong in some other place?

Thanks,

Christian

This topic has been closed for replies.

11 replies

Yohann M.
ST Employee
June 11, 2021

Dear Christian

This issue is not a known issue. could you please provide further information? How do you start from? X-CUBE-TCPP with SINK LPM application? FW G0 Package?

Anyway, I will raise a ticket internally to track this issue and come back to you.

Regards,

Yohann

CWern.1
CWern.1Author
Associate II
June 11, 2021

Hi Yohann,

I am using a STM32G071GBN. I started from the CubeMX version 6.2 with the G0 package version 1.4. I created a Source application.

For the low power handling I looked up the example project for the STM32G081b-Eval "USB-PD_Provider_1Port". And I am using the non-Os implementation.

Thanks,

Christian

Yohann M.
ST Employee
June 11, 2021

Thanks for your feedback!

In meanwhile, did you have a look at the application we delivered for Low Power in sink mode?

x-cube-tcpp/Projects/NUCLEO-G071RB/Applications/USB_PD/USBPDM1_Sink_LPM at main · STMicroelectronics/x-cube-tcpp · GitHub

Yohann

CWern.1
CWern.1Author
Associate II
July 1, 2021

Yes I did have a look at your example. I don't see a difference in the middleware files, aside from it being a sink and I have a source application. So I don't know how comparable the two projects are.

Did you have any luck replicating this behavior?

Christian

CWern.1
CWern.1Author
Associate II
September 23, 2021

Dear Yohann,

I tested the file you supplied with the old version 3.2 and the new 4.0.0 of the USB-PD library. Unfortunately no luck with both. Problem still persists.

Yohann M.
ST Employee
September 27, 2021

Dear Christian,

Is it possible to provide the project to this thread?

regards,

Yohann

CWern.1
CWern.1Author
Associate II
October 14, 2021

Dear Yohann,

yes I can share it with you. Is there any way I can get it to you?