2022-06-01 5:05 AM
I am using B-L475E-IOT01A (STM32L475VGTx) dev kit and this article for DFU and I am getting following issue.
I am using flash decription as show in the tutorial.
#define FLASH_DESC_STR "@Internal Flash /0x08000000/02*016Ka,02*016Kg,01*064Kg,03*128Kg"
For replacing flash mem read,write api I have taken a reference from STM32L476G-EVAL DFU_Standalone example.
In my driver SCB->VTOR is not set so not changed app start location.
Can anyone please suggest what could be the reason for this ?
2022-06-01 6:10 AM
I have further debugged with this using STLink. Bootloader stucks into waiting for HSE is ready or not.
Also Debugged Led App Seperately. If I start that application from 0x8000000 it works preffect but If I change address to 0x8008000 it stucks in HAL_Delay as shown below in while
2022-06-04 4:16 AM
Hey @Imen DAHMEN
Can you please help me out here.
I have been able to detect device as STM32 DownLoad Firmware Update in my device manager. But DfuSeDemo tool is not able to detect the device(B-L475E-IOT01A). I am using STM32CubeIDE as my developement environment.
I have followed this article.
@#askST Embedded World
2022-06-06 3:35 AM
Hello Community,
I have tried with STM32F469 discovery kit with example provided in STM32Cube Repo.
But result is same. My PC can detect the device but DfuSe Demo App can't.
Can anyone help me out here ?
From the UM0412 User manual, It says that
Compatible HID device is a HID class device providing the HID detach feature (USAGE_PAGE 0xFF00 and USAGE_DETACH 0x0055) in its report descriptor.
Can anyone guide me on how to use this ?
2022-06-06 6:26 AM
Hello guys I am able to detect the device in DfuSe Tool by installing the drivers.
Got the solution from this
But now I am getting this. It stucks at 24% everytime.
2022-06-07 2:44 PM
Hello @Keyur Thumar ,
Which bootloader version is used ?
Maybe that the problem is related to the bootloader version.
Please check your configuration with boot mode and the Known limitations described in the AN2606 related to your device and bootloader version.
Have you checked with STM32Programmer?
Maybe this post can help you.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
2022-06-08 1:36 AM
Thanks @Imen DAHMEN for the response.
I have followed this video tutorial and created application for bootloader. I have not used read out protection into that.
This video doesn't show any timer configuration as suggested by AN2606 - Timer 17
I couldn't found any source code for bootloader version 10.x or 9.x. Can you please provide the source ?
My bootloader code can be found here
Thanks again.
2022-06-09 12:00 AM
@Imen DAHMEN
I have checked with STM32CubeProgrammer. It can not detect my device as USB.
2022-06-09 6:38 AM
Thanks you for the response.
Now I am able to DFU on my device, but after full chip erase and bootloader flashing.
After I have done DFU once, after that I am not able to do it again. It again stucks at some random percentage. To do it again, I have to erase full chip using STMCubeProgrammer, reflash the bootloader and then I can do the DFU.
@Imen DAHMEN
2022-06-09 6:46 AM
@Imen DAHMEN
ALso I am getting errors like below in DfuSe Tool.