AzureRTOS Nx_TCP_Echo_Server on NUCLEO-H743ZI2
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-27 2:23 AM
Hello everyone,
I use the NUCLEO-H743ZI2 board in my project and previously, Before I've used the MBed OS - it works well on this board, just I need to maximize TCP transfer speed as well as QSPI. So I decided to try another RTOS. After reading forums, I decided to try the Azure RTOS and Cube IDE. I chose the Nx_TCP_Echo_Echo_Server example as a starting point. I reconfigured it to use with NUCLEO-H743ZI2, and also I disabled DHCP as I don't need it. Also added plenty of printf functions at different steps in the app_netxduo.c. As result project can be build, and I see next messages in Terminal:
The network cable is connected.
nx_ip_interface_status_check == NX_SUCCESS.
nx_ip_address_set == NX_SUCCESS.
nx_tcp_socket_create == NX_SUCCESS .
nx_tcp_server_socket_listen == NX_SUCCESS .
TCP Server listening on PORT 5000
STM32 NX_APP_DEFAULT_IP_ADDRESS: 192.168.0.200
Next is the tx_semaphore_get
Then I try to ping the board I see the blinking LED on the Ethernet connector of the board but I get :
Ping statistics for 192.168.0.200:
Packets: Sent = 4, Received = 0, Lost = 4 (100% loss),
Thus, it looks like the function
static VOID tcp_listen_callback(NX_TCP_SOCKET *socket_ptr, UINT port)
{
tx_semaphore_put(&TCPSemaphore);
}
never called.
I already spent two days trying to find solutions. All receipts which I found - like
https://community.st.com/t5/stm32-mcus/ethernet-not-working-on-stm32h7x3/ta-p/49479
I implemented them - the result is the same.
Does anyone have any idea where is the problem?
Thanks in advance.
- Labels:
-
AzureRTOS
-
Ethernet
-
STM32H7 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-27 5:57 AM - edited ‎2025-03-27 5:59 AM
You must add some more info to get valuable feedback like if you are running some demo or 100% your code.
In case you are NetXDuo primitive, try look at stats embedded in NX_IP structure.
You can get an idea if ethernet is working properly.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-27 6:04 AM
Thank you for reply!
As I am a newcomer here, could you please explain what should I upload? The whole project now is 160Mb and in ZIP it is 50 Mb - probably this is too large?
Thank you in advance!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-27 7:00 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-27 7:45 AM
I had a look at your code and:
- you did not see my post "
STMCubeMX migration to v6.13 FW H7 V1.12 " -
- LinkerScript define RxDecripSection but code use RxDescripSection; - It seems you have 2 projects nested one inside another - avoid as it make difficult to troubleshoot;
- when you share a project, delete all Debug dir - will be smaller.
I stop here - let me know if you are ok
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-27 8:10 AM
Thank you for your reply!
After correction RxDescripSection to RxDecripSection and TxDescripSection to TxDecripSection result it the same - my board do not respond to ping. Also now I got not a success return value from the
status = nx_ip_interface_status_check(&NetXDuoEthIpInstance, 0, NX_IP_ADDRESS_RESOLVED,
&actual_status, 10);
lines in the app_netxduo.c
As for the "2 projects nested one inside another " - I don't have any idea why it happened as I used the Import STM32Cube example wizard! Honestly for me this is the 2nd project in CubeIDE - first was LED blinking.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-27 9:09 AM
I loaded your code and got stuck at
HAL_StatusTypeDef UART_WaitOnFlagUntilTimeout(UART_HandleTypeDef *huart, uint32_t Flag, FlagStatus Status,
uint32_t Tickstart, uint32_t Timeout)
{
/* Wait until flag is set */
while ((__HAL_UART_GET_FLAG(huart, Flag) ? SET : RESET) == Status)
{
/* Check for the Timeout */
if (Timeout != HAL_MAX_DELAY)
{
if (((HAL_GetTick() - Tickstart) > Timeout) || (Timeout == 0U))
{
return HAL_TIMEOUT;
}
if ((READ_BIT(huart->Instance->CR1, USART_CR1_RE) != 0U) && (Flag != UART_FLAG_TXE) && (Flag != UART_FLAG_TC))
{
if (__HAL_UART_GET_FLAG(huart, UART_FLAG_ORE) == SET)
{
/* Clear Overrun Error flag*/
__HAL_UART_CLEAR_FLAG(huart, UART_CLEAR_OREF);
as if you do have a bad .ioc.
Here a valid .ioc & .ld
Generate a new project with this .ioc, replace .ld. you should be ok.
I suggest you create a new project for your board with a single project.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-28 2:42 AM
Good morning Mbarg,
Unfortunately all the magic passes :) don't work.
My previous project had not any problems with USART but you have them.
I inserted in it valid .ioc & .ld from you - this did not help. Even more - this ioc gave me next problems with Ethernet:
So I followed your advice and created a new project.
I have configured Azure as shown here.
I added a blinking LED3 like here - to know that the board is working
I changed MPU configuration according to this link.
I did correction RxDescripSection to RxDecripSection and TxDescripSection to TxDecripSection according to this link.
And finally I added app_netxduo.c and app_netxduo.h from old project.
As result - LED blinking, USART working, Ethernet initialized well, but still I can't ping my board!
And I don't know which shaman's tambourine to bang now.
Can you help, please?
Thank you very much in advance!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-30 10:57 PM
Sorry, but you did NOT follow my instructions correctly.
I asked you to generate a new project from my .iot, using STM32CubeIde menu New -> STM32 Project From Existing ... - see screenshot.
Actually your project has wrong ETHERNET GPIO Settings - Nucleo board use other pins !!
Also .ld is not what i sent - @line 141, there is no include ... and you have not my MB_H743.ld extension in your project.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-31 12:43 AM
Good morning Mbarg,
Ок, I created new project as you suggested - see it in attachment.
Just in your Azure RTOS settings, I disabled most of the Ethernet features as I need a very simple thing - TCP server with static IP address. And I inserted the content of the MB_H743.ld inside STM32H743ZITX_FLASH.ld as I have another folder structure. Also I added app_netxduo.c and app_netxduo.h from old project.
As result, the project can be build and uploaded to the board, but it restarts every second - I see it in the Terminal.
And I still do not have a chance to ping my board.
> Actually your project has wrong ETHERNET GPIO Settings - Nucleo board use other pins !!
I have looked the official document - mb1364-h743zi-c01_schematic.pdf
And yes, you are right - the two pins TX_EN and TXD0 are connected to another pins compare to official STM's ioc file for this H743ZI2 board. Strange! Why ioc file was not tested?
What I can do now?
Just as remark: I need a very simple thing - TCP server with static IP address. I use official STM's board and I do not understand why it takes one week of fight without success to do such simple thing?