2024-07-18 3:52 AM - edited 2024-07-18 11:46 PM
Hello,
My issue is related to:-
MCU: STM32H733
Middleware: Azure RTOS
Middleware Component: NetxDuo (6.2.0)
Addon: mDNS
I am using Azure RTOS with NetxDuo, I implemented a secure https server in my device and implemented mDNS which was working very well for me till I required to change domain. I want to add a sub-domain like (myhostname.mysubdomain.local). In documentation it is stated that by default the domain is .local but can be changed using following API
Now, I have implemented this API in my code like this:
```
status =
nx_mdns_create(&mdns_instance, &ip_instance, &netxduo_packet_pool, MDNS_PRIORITY, mdns_thread_stack,
sizeof(mdns_thread_stack), (UCHAR *)hostname, (VOID *)local_service_cache,
sizeof(local_service_cache), (VOID *)peer_service_cache, sizeof(peer_service_cache), NX_NULL);
if (status != NX_SUCCESS)
{
Error_Handler();
}
status = nx_mdns_domain_name_set(&mdns_instance, "home");
status = nx_mdns_enable(&mdns_instance, PRIMARY_INTERFACE);
```
It returns success and according to the document I must be able to ping hostname.home but thats not the case not matter what I done it will be always accessible through hostname.local
I checked the domain name buffer inside mdns_instance, its updated to home but even then changed domain is not accessible.
Goal: To be able to add subdomain
Bigger Picture: I want to use wild card while generating certificate and keys in alt name and CN so that same certificate can be used in many devices thats why I need subdomain as it allows wild card in *.example.local not in *.local
2024-07-19 9:08 AM
Hello @faharintisar ,
After giving it some thought, I think that this could be a problem not relaled to your MCU setting this. home instead of .local but this can be explained maybe by devices on the network still memorizing the last names in mDNS cache.
So, try clearing any mDNS cache on the devices you are using to test the domain name resolution. Cached entries might still point to the old domain.
Regards
2024-07-21 9:46 PM - edited 2024-07-21 11:39 PM
@STea Thanks for reply, Yes I tried it but unfortunately issue is still there.
2024-07-22 8:20 AM
Hello @faharintisar ,
sorry to hear this another suggestion maybe to use the API call as follows:
status = nx_mdns_domain_name_set(&mdns_instance, "hostname.home");
Regards
2024-07-22 10:51 AM
@STea Unfortunately no, https://github.com/eclipse-threadx/rtos-docs/blob/main/rtos-docs/netx-duo/netx-duo-mdns/chapter4.md
In this example they have used only domain in this api, and this is the only document and example I could find.
2024-08-14 7:41 AM
Hello @faharintisar ,
did you manage to get it working? maybe see if you can seek any help from the GitHub issues related?
Regards
2024-08-16 10:42 AM
Thanks @STea for asking, but unfortunately no...remanis unresolved
2025-02-18 2:05 AM
Hello @faharintisar ,
Could you please check the following shared file which set mDNS with NetX.
Regards