cancel
Showing results for 
Search instead for 
Did you mean: 

AZURE RTOS CDC US is not detected

MDeva.1
Associate II

Hello,

I am working on nicleo-h745ziq board according to this video https://youtu.be/wCRIpp-OHY4 i follow the steps biut USB is not get detected why? also I create project for Ux_Device_CDC_device but also in this example usb detection is failed why this happend? i try simple USB CDC as virtual comport is works fine can you please help there is any support for only AZURE RTOS

4 REPLIES 4
KDJEM.1
ST Employee

Hi @MDeva.1​ ,

Try to increase the heap size, This may solve your problem.

Also, I advise you to follow these links to know how to use the USBx for Azure RTOS applications.

https://wiki.st.com/stm32mcu/wiki/Introduction_to_USBX

https://wiki.st.com/stm32mcu/wiki/Introduction_to_Azure_RTOS_with_STM32

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

0693W00000Ns5WwQAJ.png0693W00000Ns5ckQAB.pngI make these following configuration this is right or wrong ,which paramter i have to change?0693W00000Ns5eLQAR.png0693W00000Ns5VjQAJ.png

KDJEM.1
ST Employee

You can change the heap size in the project manager to 0x500 as shown in the below figure.0693W00000Ns7JyQAJ.pngKaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

mohamed.ayed
ST Employee

@MDeva.1 ​Could you please verify your endpoint config?