2022-08-05 12:31 PM
I am using PyOCD and CMSIS Pack Manager to connect and read from my MCU. However, to write I need to know the specific MCU name such STM32g071cbux. Is there a way to autodetect that variation between like STM32g071cbTx. or can I auto detect like my pc_init, pc_unInit, pc_program_page, pc_erase_sector, pc_eraseAll, static base, begin stack, end stack, begin data, page size, page buffers address from the mcu?
2022-08-05 12:46 PM
DBGMCU should have a "DEVID" and the System/OTP should have a "FLASH SIZE" and perhaps "RAM SIZE" variable.
There's supposedly also some detail in the UNIQUE-ID but I'm not sure how publicly unpacked that is. Ask your local FAE.
2022-08-05 12:53 PM
I can find the Device ID and Flash Size fine, but some of the other addresses I can't. Do you know if like family variations are in there? Seems like I can find up STM32G0X1XX and I am missing the few X parts.
2022-08-05 1:21 PM
A lot of the part share a common die, with different bond out, or features disabled.
I think pin/package stuff can be sieved via the UNIQUE-ID, would take some effort, and I'm not interested in doing the work.
The RAM size could be probed.