2016-06-07 7:54 AM
I posted on the eval forum but after further experiments trying here.
I'm using the STM32F746G Discovery. I'm using the audio_loopback.c demo slightly modified to use line inputs instead of mics. I get lots of crosstalk/echo/ringing when I set the audio gain at any usable level. At first I thought maybe it was because of crosstalk between the input/output circuit board traces, but they are very short, and then I used an external low impedance buffer which should prevent crosstalk I would think. I had to modify the BSP_AUDIO_IN_OUT_Init routine to allow an audio input type of INPUT_DEVICE_INPUT_LINE_1 and code below suggested that would be handled even though the example disallowed that as an input. The slight delta is it uses CODEC_AUDIOFRAME_SLOT_02 instead of CODEC_AUDIOFRAME_SLOT_13. I don't have a conceptual understanding of what those slots mean. It seems like what I'm trying to do should be fairly common: take an audio input from the line inputs and output it to the line/headphone outputs. Pointers or suggestions? Thanks. #audio2016-07-12 10:29 AM
2016-07-12 11:31 AM
http://www.tjaekel.com/udante/files/STM32F769IDiscovery.zip
For the f746 disco, this example works, but lacks a line-in option. Probably the config can be figured out from the f769 example, and put into the f746 example.http://www.tjaekel.com/DiscoveryF7Audio/index.html