cancel
Showing results for 
Search instead for 
Did you mean: 

Are there plans for CAN support in open bootloader?

ben5en
Associate II

As I have seen, an open bootloader middleware is offered for the STM32G4. An FDCAN implementation can be found here. Are there any plans to also offer a pure CAN implementation?

I am also interested in whether it is possible to program directly via CAN using the CubeProgrammer and the STLinkV3? In this case it would be conceivable for me to write a CAN implementation myself based on the open bootloader.

Best Ben!

1 ACCEPTED SOLUTION

Accepted Solutions
Houda GHABRI
ST Employee

Hi ben5en,

Yes, the programming via CAN is supported by CubeProgrammer and the STLinkV3 however the FDCAN is not supported .

Hope this helps you.

Houda

View solution in original post

1 REPLY 1
Houda GHABRI
ST Employee

Hi ben5en,

Yes, the programming via CAN is supported by CubeProgrammer and the STLinkV3 however the FDCAN is not supported .

Hope this helps you.

Houda