2021-08-04 7:10 AM
As I have seen, an open bootloader middleware is offered for the STM32G4. An FDCAN implementation can be found here. Are there any plans to also offer a pure CAN implementation?
I am also interested in whether it is possible to program directly via CAN using the CubeProgrammer and the STLinkV3? In this case it would be conceivable for me to write a CAN implementation myself based on the open bootloader.
Best Ben!
Solved! Go to Solution.
2021-08-11 8:33 AM
Hi ben5en,
Yes, the programming via CAN is supported by CubeProgrammer and the STLinkV3 however the FDCAN is not supported .
Hope this helps you.
Houda
2021-08-11 8:33 AM
Hi ben5en,
Yes, the programming via CAN is supported by CubeProgrammer and the STLinkV3 however the FDCAN is not supported .
Hope this helps you.
Houda