cancel
Showing results for 
Search instead for 
Did you mean: 

1. What USB mode are supported by NUCLEO-F401RE which can be used to connect with PC 2. Can board connect as USB OTG? 3. NUCLEO-F401RE driver required for PC – Windows & Linux? If yes, are they available?

CParm
Associate
  1. Want to Know all the USB stack supported by NUCLEO-F401RE extra of Virtual COM port, Mass storage, Debug port?
  2. NUCLEO-F401RE does support OTG?
  3. Interrupt Transfer is supported by NUCLEO-F401RE or have any near future plan to support?
  4. Driver for NUCLEO-F401RE is available for Linux and Windows?
  5. We want to configure and read Real time data from from I2C/SPI slaves and send data to PC through USB. Do you have any such sample application?

1 REPLY 1
MZeh.1
Associate

Does anyone have an answer for number 4? I am also seeking Linux tools for this board. The descriptions of the downloads do not list them by OS. I am using a few different Linux types. Please post whether this is supported.