cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-LPM01A Board wrong voltage after calibration?

Roadrunner1805
Associate III

Hello,

I'm using the X-NUCLEO-LPM01A Board. Today I encountered a problem with the calibration. If I set the voltage to 3.3V and run a calibration I measure at VOUT only 3V. Without any calibration I measure the expected 3.3V. If I set the voltage to 1.8V and run a calibration I measure also 3V at VOUT. Without calibration it's 1.8V. Have you seen this problem? Or do I something wrong? Maybe I have to set the voltage after calibration again?

1 ACCEPTED SOLUTION

Accepted Solutions
Roadrunner1805
Associate III

This issue has been fixed in the new firmware version [v1.0.7] of STM32-LPM01-XN.

Here is the link to access the last one of the firmware:

https://www.st.com/en/development-tools/stm32-lpm01-xn.html

View solution in original post

2 REPLIES 2
Roadrunner1805
Associate III

This issue has been fixed in the new firmware version [v1.0.7] of STM32-LPM01-XN.

Here is the link to access the last one of the firmware:

https://www.st.com/en/development-tools/stm32-lpm01-xn.html

Great!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.