2023-07-04 7:52 AM - edited 2023-07-05 3:35 AM
Hallo.
I have NUCLEO-L476 and X-NUCLEO-GNSS2A1 (with Teseo-VIC3DA). Of course, the only one present example, in "en.x-cube-gnss1" package for both boards (GetPos) works great, but all examples (including GetPos) available in package, work with RTOS. Unfortunatly, I am no familiar with RTOS, I will also not use RTOS in my project. I spent lot of hours to analyse the code and documentation, to find the way to use VIC3DA without RTOS without succes. I know also, that many GPS modules (for example from Origin GPS...) work just after powering it, the only problem is to efficiently parse the data from NMEA frames - there will be no problem with it.
And now is the question. How to:
It should be simple, but it is not.
2023-07-07 2:42 AM
Hello @PDobr.1 ,
Thanks for trying out this package.
For Package without RTOS I suggest you start by generating the new ioc for NucleoL476RG using STM32CubeMX tool and using the settings of Virtual_COM_Port.ioc placed in X-CUBE-GNSS1\6.0.0\Projects\NUCLEO-F401RE\Applications\Virtual_COM_Port .
Generate the code and use the function TeseoConsumerTask for getting the GNSS NMEA Message and ConsoleParseTask for parsing the message. Right now they are associated with thread but you can comment that and use above functions directly.
USART1 Baud rate you can make 115200.
Let me know !
Regards,
Saurabh
2023-07-07 4:40 AM - edited 2023-07-07 5:15 AM
Hello,
thank you for the answer. Regarding the settings - I must copy ports, interfaces settings and middelware package settings (X-CUBE-GNSS1 - change for VIC3DA, without using RTOS - RTOS disabled), according to set pictures below?
- pionout and port settings for connection with X-NUCLEO-GNSS2A1 board:
- interrupts (USART):
- USART1, change BR to 115200:
- settings of GNSS1 package, we are disabing RTOS (here is still enabled, thig to change):
And the last needed thing - to use two mentioned functions (Consumer and ParseTask) - I must comment these lines marked as red in main.c --> main(), as placed below (if I want to use/modify ready example for L476 0 GetPos - from package, it has RTOS inside) :
If something is missing, please correct me.
regards, Paul
2023-07-07 5:59 AM
2023-07-07 6:17 AM - edited 2023-07-07 6:17 AM
Few more things, can you explain mi how to use these two functions (TeseoConsumerTask, ConsoleParseTask)? Where put them, in main()? They are associated with thread, so where should I put a comment to make the unassociated? And the last thing, which extensions should be chosen:
- all?
Hope it is all, what I will need t know, I will try to make it work on the weekend...
2023-07-09 9:55 PM
Hello ,
Since you are not using RTOS you have to devise your own way to simultaneously receive and parse the NMEA data.
You may call TeseoConsumerTask and ConsoleParseTask inside MX_GNSS_PostOSInit or in a main while loop.
Dont call _init ( where above two functions are associated with the thread) .
You can pass a const parameter in above two functions soemthing like : TeseoConsumerTask("GNSS Fetching the NMEA Data..!"); and ConsoleParseTask("GNSS Parsing the NMEA Data..!"); .
We haven't tried without RTOS but above sequence should work. Please try.
Regards,
Saurabh
There are osthread handlers which are .
2023-07-10 1:40 AM
Thanks for an answer. The best way, I think, the fastest one, is:
(above - commented _init functions and added TeseoConsumerTask("GNSS Fetching the NMEA Data..!"); and ConsoleParseTask("GNSS Parsing the NMEA Data..!"); )
(above - main() with added while(1);
It compiles without errors, I'll try it in the evening and send fedback - if it works or not.
2023-07-10 10:42 PM - edited 2023-07-10 10:48 PM
Hallo. Unfortunatly the solution you adviced doesn't work with NUCLEO-L476 and NUCLEO-F401 - I took code from X-CUBE-GNSS1 examples with RTOS (so, the configuration was good), there are these functions implemented, so I disabled _init and added TeseoConsumerTask and TeseoParserTask - without success.
2023-07-17 2:54 AM
Hello ,
Can you please attach your project or zip file here.
Regards,
Saurabh
2023-11-08 8:54 AM
@PDobr.1 I'm a beginner for the X-NUCLEO-GNSS2A1 module. I could not get the basic outputs even using the example application codes. Could you assist me? I have Nucleo64 - g491Re board as well.